Part Number: LMK00105 Hi,
We want to use LMK00105 clock driver IC to drive Clipped SIne wave from a ECS-TXO-20CSMV TCXO to four synthesizers. Could you let us know the suitability of the P/N that we have chosen from TI & whether it is capable to drive…
Part Number: LMK00105 Hello,
Could you please help me to ansewr the following question from my customer.
"We are considering to use LMK00105. As an input connection device for LMK00105, we are considering NB7V52M or NB4L52, but could you tell us if…
Part Number: LMK00105 Hi Team,
Customer want to know when VDD=3.3V, OE=3.3V, VDDX=0V, what is the output voltage in output pin,
Based on other E2E link, it should be 0V and what is the impedence?
If there is external power rail, the output will…
Part Number: LMK00105 Other Parts Discussed in Thread: LMK1C1102 Hi Team,
Please provide a similar IC to the LMK00105 with a 2-channel LVCMOS fanout buffer that supports a 25 MHz clock input and crystal input support.
Part Number: LMK00105 Hello,
A customer is looking for an LVDS receiver that meets the following specifications: - Rise/Fall Time:600ps(typ) - Power supply voltage: 3.3 V, 2.5 V, 1.8 V - Jitter :RMS Jitter:30fs(typ)Data rate: 200 MHz (max) - Inputs…
Part Number: LMK00105 Hello,
I received an inquiry from a customer regarding the maximum output current specification for each output.
She would like to know the maximum specified value. Could you please provide this information? If no, could you…
Other Parts Discussed in Thread: LMK00105 , LMK00804B , LMK00101 , CDCLVC1310 , LMK1C1102 We have a timing-critical clock/sync distribution application and would appreciate some clarification on a few points, or indeed get your recommendation on a better…
Part Number: LMK00105 Tool/software: Hi,
following to my schematic:
1. Are the OSCin/OSCout pins required to be left floating when operating with CLKin?
2. What shall I do with the unused clock_out pin?
3. Is a 50-ohm termination required at each…
Part Number: LMK00105 Tool/software: Hello TI Team,
We have been using OSCIN pin as a LVCMOS single ended input. We chosen this for the sync up purpose. We have a couple of queries mentioned below: 1- What is the output skew between the CLKOUT2 and…
Part Number: LMK00105 Other Parts Discussed in Thread: LMK6C , CDCM6208 hello,
i have to update an board, some parts are eol. i am not the designer from the board, that is the reason why i check every ic and the passive components.
at the board is…