Part Number: LMK00301
Hi team,
A question from my customer. The customer is doing an error/fault injection test to LMK00301. They create some faults manually and test how the fault influences the whole system.
Customer shorted one of the output…
Part Number: LMK00301 Hi dear supporting team,
if customer could only solder 50% area of the thermal pad for LMK00301, will it affect any performance ? tks!
Part Number: LMK00301
Since the time jitter performance of the LMK00301 depends on the slew rate of the CLKin signal, I would like to confirm that we are computing the input slew rate correctly.
The differential CLKin signal is the voltage difference…
Part Number: LMK00301 Hi team,
Below is the diagram of my customer's application.
The output signal of LMK00301 is LVPECL and the input signal of the PHY.
Customer use the phy to monitor the output clock of the LMK00301 , and we found when the…
Part Number: LMK00301 Hello,
I have a design w/ this buffer and I'm looking to have control over the output clock banks in order to reduce power consumption when necessary.
From the datasheet, it would seem that this could be achieved by disabling…
Part Number: LMK00301 Is the additive RMS Jitter Integration Bandwidth 1 MHz to 20 MHz for LVDS output, VCCO = 2.5V, and Clockin Frequency = 625 MHz available? I can only find the additive jitter with VCCO = 3.3V for LVDS output on datasheet.
Part Number: LMK00301 Other Parts Discussed in Thread: CDCLVC1310 Hi team,
When my customer use the LMK00301 and CDCLVC1310, there is a situation that they power off the units but remain input the clock signal in the input pin.
So my customer want…