Part Number: LMK00308 Hi Support Team,
Regarding LMK00308, I would like to know the following questions:
About 2 months after start using, one LMK00308's CLKOUTA port clock output stopped. Even if CLKOUTA_TYPE0 is pulled down to GND with 1K ohm…
Part Number: LMK00308
Hi,
we need a clock buffer/mux which is able to multiplex two input and fan out 8 output . One of the input signals is LVDS(0-1000MHz), the other is analog sine-wave(0-100MHz). The output signal should be LVDS. LMK00308 looks…
Part Number: LMK00308 Other Parts Discussed in Thread: LMK05318 Hello,
At the Clock Inputs there is a slow Clock Signal (<10MHz). Switching from one to the other Input is done when both Clock Signals are "low".
Then, switching from CLKin0 to CLKin1…
Part Number: LMK00308 Hello,
I would like to know when valid clock-out after power up.
What time does it take between power up to getting valid clock-out?
or How do we know when output clock is valid after power-up?
Best regards,
Katsu
Part Number: LMK00308 Hi Team,
I'm looking for the Junction to Board thermal resistance of LMK00308SQ/NOPB, this is not listed on the datasheet thermal resistance data. Can you also give the complete thermal resistance data of this device?
Looking…
Part Number: LMK00308 Other Parts Discussed in Thread: LMK00101 Hi,
We are using lmk00308 & lmk00101 in our design ,
1. out of the 3 clock inputs for both the IC's, we are using clkin0 only , can we leave the unused inputs clkin1 & OSCIN floating…
Part Number: LMK00308 Other Parts Discussed in Thread: LMK00304 ,
Hi All,
I am sending this email to ask some questions on input bias voltage and termination resistor of LMK00304/08.
My customer has applied LMK00304 and LMK00308 to new system and…
Part Number: LMK00308 Other Parts Discussed in Thread: LMK61E2
Hi,
We would like to use si570 to drive LMK00308 with LVDS (Vcm=1.20V) signal and we want to use as few components as possible due to space limit which means DC coupling, direct connection…
Hi,
lmk00308 output is converted to single ended using the reference circuit given snau136c.
But for lvds outputs of lmk00308 VOD = 400mv & vos=1.25V , will this be sufficient to drive OSCIn of lmx2581 which requires an AC coupled input of min…