Part Number: LMK00338 hi, Team
could you tell me what appropriate device is?
・PCIe data rate:Gen3
・PCIe amount of rane:×16
Is LMK00338 good fit with above?
Other Parts Discussed in Thread: LMK00338 hi, Team.
could you tell me subject?
it looks like they are much similar but output type is programmable which i found those different .
any other thing?
Part Number: LMK00308 Other Parts Discussed in Thread: LMK00338 , Hi, All,
Could you tell me below?
can we use LMK00308 and LMK00338 as clock buffer and redriver?
could you tell me what are those meaning between clock buffer and redriver?
As PCIe redriver…
Part Number: LMK00338 Hi Team,
We have 13 PCIe devices and want to use the same clock. But there isn't a clock buffer with so many channels.
Can two LMK00338 be used for this application? One output of LMK00338 will be connected to the input of another…
Part Number: LMK00301 Other Parts Discussed in Thread: LMK00338 , Hi
PCIE 4.0 needs to be supported with 6 or 8 clocks, so 4.0 clock buffer is needed. In addition, HSCL level output does not need external end-to-end matching.
Does LMK00301 support PCIE4…
Part Number: LMK00338 HI
I am trying to input a HCSL Clock to the LMK00338 CLKinP/N(PIN 16 ,17),direct DC coupling as shown in Figure 20 below, or need additional AC coupling capacitors?
What is the principle of AC or DC coupling?
Part Number: LMK00338 Hi,
On the top page of the datasheet, there is the description of "Additive RMS Phase Jitter for PCIe Gen3 at 100 MHz :30 fs RMS (Typical)". Does it mean that you have history that LMK00338EVM passed PCIe Gen 3 compliance…
Part Number: CDCDB2000 Other Parts Discussed in Thread: LMK00338 , LMK1D1216 Hi,
I need to distribute low-frequency clock references to multiple loads. The CDCDB2000 looks like a good candidate.
My clocks operate between 500Hz and 2MHz. Are these frequencies…
Part Number: LMK00338 Hi
my x86 platform use 85 ohm impedance for diff. signal.
In figure 20, it says 50 ohm, it can't meet 85 ohm diff impedance.
should I change termination to meet this 85 ohm impedance.
thanks