Part Number: LMK00804B-Q1 Tool/software: Hi,
We are considering a circuit that uses the LMK00804B-Q1 as a receiver to input an LVDS signal. In the circuit we are considering, we assume that the input signal to the LMK00804B-Q1 will be a differential…
Part Number: LMK00804B-Q1 Tool/software: HI BU team
My customer is developing the multi-line flash Lidar application. They need a pwm signals to fanout to the coming MOS drivers.
The PWM waveform is shown in below screenshot.
The pwm signals is 3.3V and…
Part Number: LMK00804B-Q1 Tool/software: Hello team,
Can I connect the CLK_SEL pin to the CMOS output via 1kΩ resistor like figure below?
On the datasheet, it says "Clock select input. Typically connected to VDD with an external 1-kΩ…
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B Hello,
1. Customer is requesting if it's possible to use a 1.8V Clock input with this device.
2. They would also like to "Daisy Chain" first LMK00804B output to second …
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B , LMK04828 Hello,
I have three queries regarding LMK00804B.
Following is the circuit I have been using to provide input from 25MHz TCXO (output impedance 200ohm typ) to the LMK00804B. …
Part Number: LMK00804B-Q1 hello,
my circuit design as below for your reference; now the VDDO is 1v8, the Q2 connect with FPGA I/O via two resistors dividing voltage (because the FPGA I/O input voltage scope is 1V-1.8V) ,I want to keep the FPGA input voltage…
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: SN74LVC1G74 , LMR33620-Q1 , , TPS745-Q1 Hi, in my design I use several components from texas, like: LMK00804B-Q1, LMR33620-Q1, TPS745-Q1, LSF0108QPWRQ1, SN74LVC1G74, UCC5350MC-Q1 among others. I'm…
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B Dear experts,
we got a design were a 38.4MHz TCXO with a 0.95V amplitude is AC decoupled connected to "LVCMOS_CLK". Buffer is supplied with 3V3.
Its interesting because at buffer…
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B Hello,
Below is the requirement for our design.
We have a 25MHz crystal oscillator (+/-2ppm) in our design which operates on 3.3V with 0.2V/ns slew rate. We need to generate two clock…
Part Number: LMK00804B-Q1 Hi Team,
Are the VDDO Output Supply terminals 11 and 15 tied together on the die or do they supply two separate outputs each?
Thank you