Part Number: LMK00804B-Q1 Hi,
Below are my queries.
1)The datasheet provided VOH and VOL for different supply voltages but the test current is not provided. Please provide the test current for the VOH and VOL
2)There is note given for VOH and VOL…
Part Number: LMK00804B-Q1
The datasheet for the LMK00804B-Q1 recommends the seconds circuit when using single-ended input on the LVDS port. I have two questions:
Why does it use a split termination when there is already a series termination on the source…
Part Number: LMK00804B-Q1 Dear Team,
My Customer would like to ask if Is it possible to terminate this part LMK00804B-Q1 with a 50ohm to ground (see attached diagram)?
Your inputs is highly appreciated.
Best regards, Renan
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B Hi Team,
As the TI website maintance today, I can not get more information from Web.
A customer have the inquiry below, can you clarify it?
The data sheet for the part LMK00804BQWRGTTQ1…
Part Number: LMK00804B-Q1 If you look on page 26 of the datasheet, you see that unlike a typical QFN part, this part has pads A1, A2, A3, and A4 underneath the corners. On the next page of the datasheet (p27) you see the recommended footprint has copper…
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804B , AWR1243 Hello,
I have couple of questions on LMK00804B-Q1.
First thing is, will this drive 50 ohm load? if yes then what is the VOH and VOL levels?
I'm using this in AWR1243, for Clock…
Part Number: LMK00804B-Q1 Good day.
Is it possible for one of the inputs of the LMK00804B-Q1 to accept a clipped sine-wave clock signal from a source such as a TCXO device?
What would be the best input and configuration to use when the datasheet for the…
Part Number: LMK00804B-Q1 Hi,
My customer asks us the pin treatment on Thermal PAD and A1-A4 pad.
Thermal PAD (pin17) : connected with GND? A1-A4 pin : open?
Please advise us.
Thanks and best regards, M.HATTORI
Joey,
Does the SOC have a differential HCSL input or a single ended LVCMOS input? The LMK00334-Q1 outputs an HCSL signal, and if the inputs are single ended as in your diagram, something like the LMK00804B-Q1 .
Regards,
Will
Part Number: LMK00804B-Q1 Other Parts Discussed in Thread: LMK00804 Hello,
I asked the following question in Interface devices forum. Could you give an advice about the 3-rd point?
(Is it a good idea to use a clock buffer to transfer data, because I need…