Danilo,
We can consult the chart used to design the USB2ANY-uWIRE to confirm the connections:
USB2ANY-uWIRE Chart.xls
I generated the simplified table below for jumper wiring:
FUNCTION
EVM pin
USB2ANY pin
Readback
1
3
…
Hi Ibrahim,
It would take time for the design and modeling team to generate the encrypted HSPICE model of the output driver and provide a test bench. If you have Hyperlynx (Mentor Graphics) or other SI tools, you could model and simulate the LMK04808…
Other Parts Discussed in Thread: LMK01000 , LMK01020 To whom it may concern:
We are currently programming an LMK01020 using an FPGA directly over GPIO via the Serial Data Timing as outlined on page 8 of the LMK01000 family data sheet. Although we think…
Hello Jim,
Regarding the question I asked you on Jan 18th
e2e.ti.com/.../1744008
and your reply, I asked about the status of LMK01020, 8x LVPECL outputs when GOE=L in Clock and Timing Forum, and below I've copied the Q&A
------------------------…
Other Parts Discussed in Thread: DAC34SH84 , LMK04906 , LMX2581 , LMK01000 We are in the process of testing our dac circuit board design built with a DAC34SH84. We have confirmed our power supplies, confirmed we have read/write access to the registers…
Hi Joe,
I'm afraid the adapter board is no longer available on the web. Can you try re-wiring the signal based on schematic and pinout description attached below?
e2e.ti.com/.../USB2ANY_5F00_UWIRE_5F00_users_5F00_guide.docx
www.ti.com/.../snau228…
Hi Satoshi,
If you want to get a 80MHz differential clock output from a 640MHz clock input, I suggest use clock buffer instead of PLL synthesizer.
For example, LMK01000, LMK01010, LMK01020, CDCE18005, CDCM1802, CECM1804, CDCP1803. These clock buffers…
Pradeep,
If there is no data line that may be it. Do you have the interface card connected like the attached document (see the table of jumper requirements for LMX2531)?
USB2ANY_UWIRE_users_guide.docx
Other Parts Discussed in Thread: ADS1282 , LMK01801 , LMK00101 , LMK01000 Hi,
I use the 8 chips of ads1282 with 4.096M. I need to sample with 96 Hz so I make 96 frequency source to synchronic the ads1282 on the pluse-sync mode. I found it takes
too…