Part Number: LMK03318 Hi,
I am using LMK03318 to generate several AC-coupling LVDS clocks to one controller. Right now, two reserved clocks are not useful. Should I disable the two outputs or continuedly to generate clocks from that two output? Which…
Part Number: LMK03318 Hey,
We would some help to understand how we can change the base adresse.
We have everything configured and its working as expected - we create a epr which we are using to program the pll.
According to the datasheet we would need…
Part Number: LMK03318 HI Support,
1) Is "Export HEX register values" file generated by TICSpro the correct production programming file that should be used to program LMK03318 in production on virgin boards (using onboard I2C bus master for example…
Part Number: LMK03318 HI
Are device function parameters and reliability NOT AFFECTED if device would operate driven by LVCMOS 3.3V 25MHz oscillator 50R output impedance connected to the PRIM_P input of LMK03318 configured as shown below:
Thank you, …
Part Number: LMK03318 Hello, TI support team.
Differential output pair 0 connects to FPGA as the below circuit. R01, R02, R03, R04 = N.P. (N.P. = Not Populated) C01, C02 = 0.1uF
Q1. Does LMK03318 have the register to adjust slew rate of differential…
Part Number: LMK03318 HI,
This is related to prev case CS1525439
1. For ROM mode, the GPIO[5:0] = 24d = 0b011000, what is the value for REFSEL (2state)? The document stated REFSEL Vim =0.9V for SEFREF selection for 3state. How about 2 state ?
I am using…
Part Number: LMK03318 Other Parts Discussed in Thread: LMK03328 Hi Expert,
We find there is similar discussion for this topic in the forum,
But we want to know whether there is testing data or datasheet updated plan for LMK03318/28 supporting PCIe Gen5…
Part Number: LMK03318 Hi, i need to program the LMK03318 to be able to generate a 100Mhz, and 156.25mHz LVDS clock output. Can u let me know what the settings should be for the LMK03318 IC ? I check on the ROM Content (GPIO[5:0] = 24 , 011000, may be…
Part Number: LMK03318 Dear team,
Is there any register setting can slow down rising/falling time?
Slew rate now is too Fast, we want to increasing rising time.
If we cannot change by SW, could we add serial capacitor to increasing rising time?
Regards…
Part Number: LMK03318 Hello expert,
My customer would like to know the questions below, would you kindly help on it?
CLK GEN LMK03318 output_P and output_N can output the same frequency? (single end)
can the pin status0 and status1 of LMK03318 be used…