Part Number: LMK03806BEVAL Other Parts Discussed in Thread: USB2ANY , DS250DF410EVM , Hi,
Interfacing the evaluation kit with the PC via the USB2ANY device gives an error.
When trying to upload firmware version 2.9.1.2 to the USB2ANY device, the…
Part Number: LMK03806BEVAL Other Parts Discussed in Thread: LMK04806 , LMK03806 Tool/software: Hi,
Customer is evaluating EVM for from 12MHz~25MHz output clock.
In the TICS pro, it shows 25MHz and 12MHz but they are actually 5.2% higher than calculation…
Part Number: LMK03806BEVAL Other Parts Discussed in Thread: USB2ANY Tool/software: Hello We are trying to use the evalution board's chip with the Usb2any interface but we don't have the uwire connection board.Since the mappings are given for uwire design…
Part Number: LMK03806BEVAL Hello there,
I've been working on LMK03806BEVAL as a reference clk for SerDes applications.
While carrying out some frequency-domain measurements on the CLK outputs of the EVB, I have found that there are harmonics of 100MHz…
Part Number: LMK03806BEVAL Other Parts Discussed in Thread: USB2ANY Hi there,
We recently bought an LMK03806BEVAL , but there was neither a ' USB2Any ' adapter nor a ' USB2Any - uWire converter' in the kit. There was only a serial cable (LPT).
But…
Part Number: LMK03806BEVAL Hello,
My customer wants to see if the setting file below works on the LMK03806BEVAL and check the EVM output waveform.
However, they do not have the EVM and are unable to pruchase it now.
Could you please provide the…
Part Number: LMK03806BEVAL Other Parts Discussed in Thread: CODELOADER Hi there,
I've recently brought-up an LMK03806B EVB and have managed to automate the process using LabView - to open TICS Pro, Load a config (.tcs) file etc.,
I know that LED D3…
Part Number: LMK03806BEVAL Other Parts Discussed in Thread: USB2ANY-UWIRE We recently received the LMK03806BEVAL. We have connected to it using the included USB2ANY-uWire adapter but have been unable to interface to the evaluation board. the Eval manual…
Hello,
From datasheet 8.6.7.3 for SYNC_PLL_DLD: "By setting SYNC_PLL_DLD a SYNC mode will be engaged (asserted SYNC) until the PLL locks." Set as desired for your application.
From datasheet 8.6.6.2 for SYNC_POL_INV: "Sets the polarity of the SYNC…
Part Number: LMK03806BEVAL Other Parts Discussed in Thread: USB2ANY , LMK03318 , LMK03806 Hi there,
I am currently evaluating LMK03806B clock module using LMK03806BEval.
I am able to program the EVM using USB2Any (although there are issues with the…