Part Number: LMK05318B Other Parts Discussed in Thread: LMK5C33216 , LMK5B33216 , LMK05028 , LMK5B12204 , LMK04033 , LMK04000 , LMK04001 , LMK04011 , LMK04010 , LMK04002 , LMK04031 , LMK04610 , CDCE813-Q1 Hi team:
I would like to confirm whether we have a low consumption…
Other Parts Discussed in Thread: LMK04033 , LMK04803 I have a question regarding the LMK04033B. We’re going to be utilizing it to clean up a CPRI reference clock that is recovered from a received serial datastream coming into an FPGA. The clean signal will…
Hi Daniel,
to get both of these frequencies out at the same time, the VCO frequency must be an integer multiple of 2000MHz (for integer-N PLL). As such, LMK04832 cannot support.
Do you need jitter cleaning function? LMK04821, LMK04033 and LMK04133 can…
Hi Nicholas,
First, you said that you are using the micro wire interface. To clarify, does that mean you're using the USB2ANY-uWIRE bridge adapter? Or are you directly connecting the USB2ANY to the EVM uWIRE header? uWIRE and USB2ANY have different pinouts…
Hi Charles,
Here is an example how to figure out how to get your output frequencies using the Clock Design Tool, then configuring in Codeloader. Please let me know if it is unclear. Thanks!
LMK04033 example.docx
Other Parts Discussed in Thread: LMK04033 , LMK04826 , LMK04821 Hello,
We are in the process of redesigning a couple of our boards and presently use the LMK04033. The problem we are running into is the synchronization function that allows the aligning of…
Other Parts Discussed in Thread: LMX2581 , LMX2541 , LMK04033 Does TI offer a fractional divider clocking device?
Specifically, I would like to input an ultra-clean 122.88MHz TXCO that gets divided down to a 10MHz output clock. This 10MHz output clock would…
Hi Noel,
There is another problem about clock, there are two different frequecy of output? the frequency of one output is 10MHz and another is 100MHz, and fhe frequency of the reference and external VCXO are 10MHz, which chip can be used to realized the…
Other Parts Discussed in Thread: DAC5689 , LMK04033 I have a customer who is using the DAC5689 on an existing production board. He configures the device to be in half rate bus mode. He used both data buses and hios issue is when CLK1 is at 200MHz, CLK2…
Other Parts Discussed in Thread: LMK04000 LMK04000 family's evaluation board schematic picture is not clear to see component How can I find clear picture of EVB schematic and second question is there are two ref. clock in(CLKin0/CLKin1) for lmk04033b…