Part Number: LMK04368-EP Other Parts Discussed in Thread: LMK04832 Tool/software: Hi,
This is Dinesh from iWave Global. I have a doubt regarding the use of LMK04832 clock file in LMK04368 Clock Synthesizer. Please confirm this if we can use. Regards…
Part Number: LMK04368-EP
Hello,
My customers is currently looking for a mechanical sample. I would appreciate it if you could let me know whether the product is available and advise the part number.
Best regards,
Somehow, the table in the datasheet (SNAS840 – MAY 2023) is completely wrong. The implementation of pin-mode selection in LMK04368-EP inherits from a previous generation device, LMK04828. The table for LMK04828 is also valid for LMK04368-EP. I have included…
Part Number: LMK04368-EP Tool/software: Hello,
Does the device above require programming on each power on? Does it have any memory between power cycles?
Thanks!
Part Number: LMK04368-EP Other Parts Discussed in Thread: LMK04828 Tool/software: Hi,
I'm trying to use this LMK part in a single-loop zero delay configuration. After programming I have a 300MHz sine coming into the OscIN port which should be compared…
Part Number: LMK04368-EP Tool/software: Hi,
I want to have a 4-wire SPI interface, instead of the default 3-wire.
In this case, I understand that I should change Bit 4 of Register 0x000 to "1" (3-Wire Mode Disabled").
1.) Does SDIO (pin 52) changed…
Part Number: LMK04828-EP Other Parts Discussed in Thread: LMK04368-EP Hello,
I can find the EVM User's Guide for the LMK04368-EP on TI.com as shown below. However, the LMK04368-EP device is not found.
LMK04368EPEVM User's Guide
Is it because it…
Hi Juzer,
It is not available. For functional evaluation, you can use the LMK04832EVM. Please note LMK04832 and LMK04714-Q1 has different package.
The LMK04368-EP is package and pin compatible with LMK04714-Q1. The eval board of LMK04368-EP is available…
LMK0482x devices (LMK04821, LMK04826, LMK04828) do not support CLKINx to PLL2 reference path. This feature was added in LMK04832 and subsequent derivatives (LMK04832-SP, LMK04832-SEP, LMK04368-EP, LMK04714-Q1).
If only PLL2 is used in LMK04828, the…
Hi Maharajan,
The LMK04368-EP can be used as an exact drop in for the LMK04714-Q1. The only difference is that the LMK04368-EP has a wider temperature range than the LMK04714-Q1 (-55C to 125C instead of just -40C to 125C), due to it being rated as a…