Part Number: LMK04610 Other Parts Discussed in Thread: LMX2820 hello
I have a question concerning the input clock for the LMK04610.
Please provide the recommended specifications for the oscillator in the following configuration: 1.Phase jitter 2.Rise…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK04832 Our TI contacts are currently out of office, so I wanted to create a ticket to see if we could get a reply back while they are out. Pasting my original email to our contacts here:
We have…
Part Number: LMK04610 In my design, I am using LMK04610, with 100MHz input having phase noise profile as attached. I have two configurations:
Output1 = 500MHz, Output2 = 250MHz, Output10=200MHz
Output1 = 312.5MHz, Output2 = 156.25MHz, Output10=200MHz…
Part Number: LMK04610 Hi TI Team,
We are using LMK04610 for a CPRI application.
We want to use fast lock feature.
For this I can see that the fast lock specific Int and Prop CP values can be programmed in the device registers. I would like to understand…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK04828 , LMK04832 Tool/software: We are using an LMK04610. We have a VCXO with good phase noise specs being locked to a very stable MEMS oscillator using PLL1. Both are 100M.
We’re aware that…
Part Number: LMK04610LMK04610 is not shown in Pllatinum SIM software, so how to calculate loopbandwidth, In Tic's pro they are just asking to mention bandwidth
why pllatinum sim does't have lmk04610, then how to get overall phase noise and rms j…
Part Number: LMK04610 Other Parts Discussed in Thread: LMX2820 , LMK04208 We have a requirement of clocking high speed ADC on an FPGA SoC Clock requirement are as follows:
1. Sampling clock for ADC: 2GHz or 4 GHz, 1 output
phase noise profile for…
Part Number: LMK04610 Tool/software: Hi, I am trying to use the LMK04610 for the following setup in the Frequency Planner of the TICS Pro software:
I don't see any reason why this would not work. Are there any limitations for the Frequency Planner…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK04616 Tool/software: Hi team,
i'm using the clock distributor LMK04610 for a new project.
In the following picture there is the electrical schematic that i devoloped for the reference clock…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK04828 , , LMK04832 , LMX2572 , LMK1D2104 Tool/software: The answer record on the LMK04828: LMK04828 vs LMK04610 post states that the LMK04610, " skew across outputs can be around 100s of ps across…