Part Number: LMK04610
HI Derek,
I posted a question regarding single shot sysref generation . I am just writing this to say the device is working and the reason from my problem is sysref was being sent to a my fpga via decoupling caps. This caused…
Part Number: LMK04610 Hi:
I'm trying to understand the requirements to get a deterministic skew from input-to-output on an LMK04610 using PLL2-only mode. The overall clocking architecture we have is pretty simple, in that the output clocks needed are…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK1D2104 Hi TI team,
I have a generic question on the JESD204 interface for the Multi-chip synchronization.
Let's say, I'm using LMK04610 timing device in our application.
The DEVCLK and SYSREF…
Part Number: LMK04610 Currently we are using the LMK04610 in our design, we are using the SIT3808AI-CF-33EM-50.000000X as VCXO and the DSC1101DL5-050.0000 as CLKIN1. At the CTRL_VCXO there is a 100nF capacitor. What we see is that the PLL1 lock-detect…
Part Number: LMK04610 Currently we are using the LMK04610 in our design, we are using the SIT3808AI-CF-33EM-50.000000X as VCXO and the DSC1101DL5-050.0000 as CLKIN1.
At the CTRL_VCXO there is a 100nF capacitor.
What we see is that the PLL1 lock…
Part Number: LMK04610 Hi,
I am using lmk04610 on my own pcb. i am trying to configure it with my FPGA Arm core through software with SPI.
I can see that write and read are working great.
what i am trying to do is to lock PLL2. as much as i can see…
Part Number: LMK04610 Hello everyone.
I have correctly configured LMK04610 IC. It has on its two inputs 40MHz from KEYSIGHT 33600A double channel generator. I also used VCXO
ABLNO-V-122.880MHz. Output frequency on nr 5 output is about 10MHz (its convenient…
Part Number: LMK04610 I am trying to use the LMK04610 to generate a SYSREF pulse on one of the output clock pins. I am currently using the part in bypass mode (no PLLs activated, just outputs a copy of the input clock). From what I understand, in order…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK04616 We are attempting to use the LMK04610 to synchronize to a reference source with a low phase noise VCXO and then distribute it.
We want to support 2 reference input frequencies of 10MHz…
Part Number: LMK04610 Other Parts Discussed in Thread: LMK04828 , LMK04832 Dear sirs,
I am working in a new design and I need to simulate the phase noise of outputs of LMK04610 and I have not found any simulation tool in TI to perform this simulation…