Part Number: LMK04616 I have a board with LMK04616 and a 100 MHz fixed frequency oscillator ( CCLD-033 ) connected to the OSCin port. This is design choice of an external hardware vendor, so don't ask me about that.
There can be 2 variants for the output…
Part Number: LMK04616 Hi,
I want to use a GUI interface to configure a LMK04616ZCR present on homemade board through an SPI interface. I am just requesting a usable link to download TICSPRO SW correctly because the link on the website lead me to a bad…
Part Number: LMK04616 Tool/software: Hello,
We are using Clock Jitter Cleaner LMK04616ZCR component on our design in production.
We have observed a drift of the locking time vs temperature
As shown in the graph here below, we have measured the locking…
Part Number: LMK04616 Hi
As I know, temperature change the delay between ClkinX to ClkoutX.
Question: If I am using two devices, Is it true to say that as the temperature change (same In both devices), the delay from ClkinX to ClkoutX change and move…
Part Number: LMK04616 I would like to ask for clarification of the use of RESETN. On page 58 of SNAS663B (section 9.5.1) we are told to "Toggle RESETn pin High-Low-High" before programming. I have three related questions:
How long does RESETN need…
Part Number: LMK04616 Other Parts Discussed in Thread: LMK04828 , LMK04906 I have an application where I need to halt one of two clocks for a while (during a complex IO reset process) and then bring the clock back synchronously with the other clock (which…
Part Number: LMK04616 My system based on LMK04616 generates 1000 MHz and 250 MHz clock output is HSDS.
Clock distribution path is PLL2 VCO (= 6 GHz : 3) -> 2 GHz
WCLK = 1GHz (divided by 2)
CLK = 250 MHz (divided by 8)
I am not able to issue 250ps…
Part Number: LMK04616 Hi,
I have a custom PCB using LMK04616 and I want to trigger SYSREF pulses on the rising edge of SYNC. I have the SYSREF registers set up correctly because I can trigger SYSREF pulses by setting the GLOBAL_SYSREF bit in GLBL_SYNC_SYSREF…