Part Number: LMK04803 Tool/software: Hi, TI team:
In 0-Delay Single PLL mode, can the output still be used as feedback output if it is turned off?
The detailed settings are shown in the figure below.
By the way, if I need to align the output phases…
Part Number: LMK04803 Tool/software: Hi team,
This is FAE Jayden, my customer is using LMK04803BISQX, and they have some questions that need to reach out to you.
1) As described in datasheet, Pin 62 and Pin 63 can be configured as LOS status indictor…
Part Number: LMK04803 Hi support team.
I received a inquiry from my customer about TICSPRO setting.
I am trying to set HOLDOVER_TYPE on the user control tab in TICSPRO.
Selecting the indicated description (open-drain output) sets the corresponding…
Part Number: LMK04803 Hi
I tried to write data 0x0006 to R0 register ,but I couldn't write by figure1 . I could write by figure 2 .
Only R0 couldn't be written by figure1. Another R1~R31,I could write.
Do you have some conditions to write R0? or…
Part Number: LMK04803 Hello
I designed LMK04803 board, and the registers generated byTICS Pro. PLL2 is not locked.
Input clock frequency: 40MHz,COMS;
Output clock frequency:80MHz, LVDS, x10;
Mode:PLl2,Int VCO, 0-Delay。
The HEX-file generated…
Part Number: LMK04803 Other Parts Discussed in Thread: PCM1792A , LMK1C1104 Hi,
first of all this is a great chip!
In order to optimize LVCMOS series termination I like to know the LMK04803 clock output impedance but can't find it in the product sheet…
Part Number: LMK04803 Other Parts Discussed in Thread: CDCM6208 Hello support team,
I have a clock generation requirement as below.
Clock output 1: 74.25 MHz (LVDS 2.5 V)
Clock output 2: 125 MHz (LVDS 2.5 V)
Clock output 3: 25 MHz (LVDS 3.3 V…
Part Number: LMK04803BEVAL Other Parts Discussed in Thread: LMK04803 , LMK04832 Hello support team,
We are planning to use LMK04803 clock synthesizer IC to provide reference clock to TLK2711 SERDES transceiver. I am looking for the schematic of the…
Part Number: LMK04803 Hi,
This part is ideal for my application as I can use it to generate 1GHz, 2GHz and SYNC pulses. If I could reconfigure it as a reference jitter cleaner too that would be perfect. Is this possible?
Part Number: LMK04803
Hi all Would you mind if we ask LMK04803? <Question1> On the datasheet P88, there is the description, "8.6.3.13.3 PLL2_CP_POL, PLL2 Charge Pump Polarity PLL2_CP_POL sets the charge pump polarity for PLL2. The internal VCO requires…