Part Number: LMK04806 I have unused clock ports. Can you confirm if I need to terminate them, or just a disable in the firmware will be enough. I am using this part number: I am using this part number: LMK04806BISQE/NOPB
Part Number: LMK04806 Hi Team,
I have a customer currently evaluating the LMK04806 who is looking for a more cost-optimized solution.
The key requirements for the replacement are:
Lower cost compared to the LMK04806
Output channel: Minimum of…
Part Number: LMK04806 Tool/software: Hi TIer
With the previous optimization, we changed the frequency of the phaser, which helped to increase the 64M clock alignment, but did not completely solve it. 1, When sync signal to the PLL, which clock be locked…
Part Number: LMK04806 Tool/software: Hi Ti experts,
There is a phase noise in frequency domain from 20kHz on CLKout3 port. There is only one chip that has issue. Normal altitude is -120dBc, wrong value is -110 or -115.
When customer reconfig all the…
Part Number: LMK04806 Tool/software: Hi Ti experts,
My customer is using LMK04806 in vector signal generator product.
Now customer met function abnormal issue when using extruded top heat dissipation silicone for heat dissipation.
Though this…
Part Number: LMK04806
Hi Ti expert,
My customer is using LMK04806 to output many kinds of clocks to other DACs and FPGAs. Input clock is 100MHz.
Customer finds that there is a 1.2G phase noise as below, which can be solved by replace a new LMK04806…
Part Number: LMK04806 Other Parts Discussed in Thread: SN74AUP1G14 Tool/software: Hi experts,
My customer wants to use LMK04806 in Vector signal source project and use a OCXO input for CLKIN1. Clock wave is a sine. Test the signal of CLKout3. Frequency…
Part Number: LMK04806 Dear Expert
1. The reads and writes of register R0 are inconsistent (write 0x00145000, read back 0x80000320), and the reads and writes of other registers are consistent. The order of writing to register is from top to bottom according…
Part Number: LMK04806 Hello,
My customer used the LMK04806 as high speed data converter clock gernerator.
They has an issue of the phase noise degradation of the output clock 491.52MHz as shown below.
Please advise on the cause of the phase noise…
Part Number: LMK04806 Dear Expert
In the process of debugging LMK04806, we met two problems, we would like to ask the original factory to help solve them. The detailed description is as follows:
1.PLL output cannot be locked, and LD_STATUS(PLL2_DLD…