Part Number: LMK04816 |TSKEW| number shows CLKoutX to CLKoutY skew (LVDS) of 30ps typical. Does this apply to only the to clocks in the same clock group, or does it apply between clock group?
For example, what is the typical and maximum expected skew…
Part Number: LMK04816 Other Parts Discussed in Thread: LMK04828 , LMK04832 Hi,
Could you check below structure and recommend better device if it's available?
LMK04816B(Master): 10MHz x4, 25MHz x2, 50MHz x2, 156.25MHz x2
LMK04828(slave, cascade)…
Part Number: LMK04816 Tool/software: Hello,
What do you currently recommend for an eval board to test LMK04816? I see LMK04816BEVAL but run into an issue connecting the parallel port to a computer. I found the USB adapter USB2UWIRE-IFACE but that is…
Part Number: LMK04816 Tool/software: Hi,
We have a board using the LMK04816, and due to an error the chip was supplied with 5V instead of 3.3V. We have rectified the issue and will replace the chip itself but need to know if the digital outputs (pins…
Part Number: LMK04816 Hi,
Engineer is working on LMK04816BISQE/NOPB SI simulation and not able to find the selection that set pin 39 and 40 OSCOUT10 to LVDS or LVCMOS.
IBIS model selector only shows LVPECL. Could you help to rectify this issue ? …
Part Number: LMK04816 If I would to like to use external VCO for PLL2, do I still have to comply to 2370 to 2600MHz range in Clock Design Tool?
Or I can choose any VCO with frequency range from 1kHz to 3100MHz as stated in fFIN in datasheet?
Part Number: LMK04816 How many cores are LMK04816 internal VCO having?
Can I access to the range info for each core?
I would like to avoid locking to boundary of 2 VCO cores and causing inconsistent result after each VCO calibration because of choosing…
Part Number: LMK04816 Other Parts Discussed in Thread: LMK04906 Hi,
Can I use the digital delay on top of the 0-delay mode in the feedback clock to obtain phase advance of other outputs compared to input clock?
Part Number: LMK04816 As I know, the primary goal of 0-delay is to maintain a fix delay between CLKin and CLKout in dual-loop mode or maintain a fix delay between OSCin and CLKout in single-loop mode. That is, the delay is not zero but is a deterministic…
Part Number: LMK04816 Other Parts Discussed in Thread: LMK04805 , LMK04808 I am trying to derive a 150 MHz and 125 MHz signal from a LMK04816 that is input with a 50 MHz reference clock. When I run TICs Pro, it indicates that the PLL2 output is bounded…