Other Parts Discussed in Thread: LMK04816 , CODELOADER SIR:
I use LMK04816 in my design for the first time in my design. I encounter some problems that is puzzled me.
I reset the device through the configure of register R0, then I configure register R0…
Other Parts Discussed in Thread: LMK04906 , LMK04816 , LMK04806 , LMK04828 Hi,
for jitter cleaning and clock generation we are currently using an LMK04906 in our design (0-delay dual pll mode). I am now looking for an alternative chip that has more outputs…
Other Parts Discussed in Thread: LMK04816 Hello,
I need to drive CLKin0 of the LMK04816 with an output that uses CML (SY58040U).
As the input clock may be very slow (down to 1kHz), I think I need a DC-coupled connection from the SY58040U-output to the…
Other Parts Discussed in Thread: LMK04816 The LMK04816 datasheet, Section 3.1 Absolute Maximum Rating does not have information on maximum rating for Digital Input pins (uWire bus). So, what is the maximum current through those pins or any pin in a powered…
Other Parts Discussed in Thread: LMK04816 Hello,
I am using the LMK04816 to translate any input frequency in the range of 10kHz up to 100MHz to a output frequency that is an iteger multiple of hte input frequency and >10MHz.
The LMK04816 is configured…
Other Parts Discussed in Thread: LMK04816 sir:
I use LMK04816 clock output in LVPECL.
(1)The termination for dc coupled differential operation and ac coupled differential operation is different. while the dc coupled operation terminate to Vcc-2V, the…
Part Number: LMK04906 Other Parts Discussed in Thread: LMX2492 , LMK04816 , LP5912 Hi,
The LMK04906 datasheet gives a phase noise plot on page 108 comparing OSCout/CLKout VCXO and VCO phase noise performance. Is this measurement taken as described on page…
Jim,
Is 0x0000 value correct for 0x130 reg in that use case? Anyway, with both non-zero and zero values I still have nothing at my DAC output.
At the same time I believe that my power is OK (provided according to datasheet, checked with voltmeter), DACCLK…
Part Number: CDCVF2505 Other Parts Discussed in Thread: LMK04816 , CDCI6214 HI, staff
I'm looking for a feature equivalent device.
ispPAC-CLK5312S (Lattice) is looking for a substitute for EOS.
The requirements are ・ Input frequency: 44 MHz (※ It can…
Part Number: DAC38RF89 Other Parts Discussed in Thread: DAC38RF82 , LMK04816 , Hi!
I am using the DAC38RF89 . DACCLK frequency is 328 MHz, DAC clock frequency is 7872 MHz.
There is a problem when I 'm trying to implement Figure 141 (refer to DAC38RF82 datasheet…