Part Number: LMK04832-SP Other Parts Discussed in Thread: SN54LVTH162374-SP , Tool/software: Is there any way to increase the 11 delay steps applicable to sysref distribution path?
Part Number: LMK04832 Other Parts Discussed in Thread: LMK04828 Tool/software: We have a LMK04832 on the board and like to get all clock outputs aligned between LMK04832 (or boards).
1. LMK04832 can be in single loop or single loop 0-delay mode.
2. …
Part Number: LMK04832 Tool/software: Question on Power Down function. If I was normal mode and then I assert power down function thru Register 0x002. How do I bring up the chip back from Power down mode? Do I need to follow a power up procedure where…
Part Number: LMK04832 Hi,
As shown in the figure below, if the output clock edges of LMK need to be aligned with the reference, do you need to trigger SYNC EVENT?
If there are multiple parallel LMKs, the reference is 10MHz, and the configuration is as…
Part Number: LMK04832 Other Parts Discussed in Thread: LMK04828 , Hi:
Question 1: Can one LMK04828 DCLKoutX drive LMK04832 CLKin0 with DC-coupled differential LVDS signaling?
Question 2: 560 ohm resistor is required in LMK04828 when using AC coupling LVDS…
Part Number: LMK04832 Hi,
I'm following onto this post here: https://e2e.ti.com/support/clock-timing-group/clock-and-timing/f/clock-timing-forum/1219876/lmk04832-help-getting-synchronized-clock-outputs-in-multi-lmk04832-setup/4606427?tisearch=e2e…
Part Number: LMK04832 Tool/software: Hi
We are using LMK04832 in design,
CLKIN0 - 10MHz (OCXO), DC Coupled Input as shown in below circuit,
PLL1 Led doesn't come up, assuming PLL1 fails to Lock, But PLL2
OSCIN- 100MHz VCXO (Differential)
DC Coupled…
Part Number: PLLATINUMSIM-SW Tool/software: Hi everyone,
I am unable to download the Sim tool, when I try doing it, it seems like the link to it is broken. Any idea how I could solve the issue and install the app ?
Thanks in advance,
Have a nice day…
Zhu,
Having a 3 meter cable will lower the amplitude of the LVDS signal and cause more reflections from the transmission line. Please use the .ibs models on both products pages (LMK04832 and LMK1D2102) to determine the correct series resistance values…