Part Number: LMK04832-SP Tool/software: Dear team,
Kindly confirm the maximum output frequency which we can generate continuously using the LMK04832-SP.
Part Number: LMK04832-SP Other Parts Discussed in Thread: LMK04832-SEP Tool/software: Dear sir,
In my application, I am using LMK04832-SP part. In LMK04832-SP datasheet there is no data regarding Frequency Planning.
But while checking the LMK04832…
Part Number: LMK04832-SP What is the recommended decoupling capacitors and their values after the ferrite for LMK04832-SP when the regulator is not on the same CCA as the device for the clock outputs such as Vcc2_cg1, etc? Their are multiple caps on the…
Part Number: LMK04832-SP Hi,
Could you provide the guidance on PLL unlock issue with specific VCXO?
the issue is as below.
no issue(CPout 1.4V~2.3V swing) with 603281 from Crystek
PLL unlock issue(CPout 3.2V continous output) with MCM8730 from…
Part Number: LMK04832-SP Other Parts Discussed in Thread: LMX2615-SP , AFE7950 Tool/software: Dear Team,
Kindly share the electrical characteristics(Voh,Vol,Vih and Vil) of the LVDS Clock output (RFout) of the part LMK04832-SP.
Regards,
Mithuna…
Part Number: LMK04832-SP Tool/software: Hello,
My customer has some questions about the LMK04832-SP exposed PAD.
Q1. Is gold plating a mandatory recommendation when designing a PCB for exposed PAD?
Q2. What is the recommended solder contact ratio…
Part Number: LMK04832-SP Dear team,
I am using the LMK04832-SP part and VCXO as Clk input.
I am using the DC coupled LVCMOS input as CLKIN,whether CLKinX* input should be directly connected to GND or through capacitor for DC Coupled input option.
Part Number: LMK04832-SP Tool/software: Hi Team,
I am investigating the radiation report for the LMK04832-SP Single-Event Effects when I see this plot below.
Based on this plot? Does this mean the holdover mode works to keep the clock outputs on…
Part Number: LMK04832-SP Other Parts Discussed in Thread: LMX2615-SP
Tool/software:
Hello,
My customer has some questions about the -SP device footprint design.
Q1. Could you please provide recommended footprint information or related materials…
Part Number: LMK04832-SP Hello,
Can you guide me how to calculate power dissipation of the LVPECL emitter resistor with value of 240 Ohms/ 120 Ohms. Space grade resistors comes in power rating of 50mW and 150mW in 0402 footprint.
I followed the information…