Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04832 , LMK1D1204 Hello,
I am evaluating the LMK04832EVM and need a verified TICS Pro configuration file ( .tcs ) for a pure clock distribution setup.
I want to completely bypass all internal…
Part Number: LMK04832EVM Hi Tech,
PN#LMK04832EVM
1pcs from PO#029-FY977 with D/C 2545 & Lot Code 5021665SVT
Our customer has encountered an issue during operation: out of its14 channels, 6 channels are producing no signal output, and 2 channels…
Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04832 , Hi,
I'm trying to achieve phase synchronization across multiple LMK04832 devices, as described in Phase Synchronization with Multiple Devices and Frequencies (Rev. A)
As a proof…
Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04832
What is the purpose of the LMP7731MF/NOPB (U6) being installed on this EVM?
Since CPout1 ranges from 0 to 3.3V, the output of U6 is expected to be 0V.
Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04832 Hi TIer
My customer using the LMK04832EVM to output 2ch 40MHz from 2 dividers , and then they want dynamically to modify the registers and set output 80MHz, but wants to maintain latency…
Part Number: LMK04832EVM Tool/software: Hi team,
A customer is looking to generate low jitter LVDS from internal 122.88Mhz VCXO using the LMK04832EVM.
I would like to know best PLL and internal filter setting to achieve 300Mhz frequency from 122…
Part Number: LMK04832EVM Hi,
I am using the LMK04832LVM evaluation board . I changed the clock divider values from the default configuration to meet my requirements. The clock distribution frequency is 3200 MHz . I am not using all SYSREF outputs (SCLK_out…
Part Number: LMK04832EVM Tool/software: I wish to use LMK04832EVM in single loop mode, where a single-ended clock source is input into the OSCin port.
The EVM user guide says "An external VCXO may be optionally attached through these SMA connectors…
Part Number: LMK04832EVM-CVAL Other Parts Discussed in Thread: LMK04832 Tool/software: Hello! The LMK04832 Datasheet claims "15-bit address field (A14 to A0) and a 8-bit data field (D7 to D0)" (section 8.5), but the registers listed only span 0x000 to…
Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04832 Hi team,
I want have two clocks with LMK04832EVM , one is 6.25M ,another is 16×6.25M 。and the two clocks have 90° phase difference.can you show me how to configure it. thanks.