Part Number: LMK05028 Other Parts Discussed in Thread: USB2ANY Hi,
We have ran into trouble with the LMK05028 and having it locking on to reference clocks and switching in between them.
We are running the LMK05028 in EEPROM + SPI (Soft pin mode) and…
Part Number: LMK05028 Hi team,
My customer is evaluating the LMK05028RGCR as their IEEE 1588 synchronizer, do we have any spec requirement for the TXCO? or recommended TXCO solution?
Thanks
Part Number: LMK05028 Other Parts Discussed in Thread: LMK5B33216 , LMK5C33216A , Hi team,
Would you please kindly help recommend to compete with AD9545? I didn't see related fighting guide at seismic, so reach out for support!
B R,
Owen
Part Number: LMK05028 Hi,
I would like to ask for your assistance with 2 points about clock generation using the LMK05028 as below.
Q1) In 2-Loop TCXO-DPLL mode, when generating a clock, I understand that the output clock ahould be dependent on the…
Part Number: LMK05028 Tool/software: On the circuit, the 'LMK05028' and the oscillators (XO, TCXO) mentioned below are installed. Ref_IN1 is fed with 5MHz (LVCMOS). We want to synchronize 125MHz (Out0) with REF_IN1.
Several tests were done by different…
Part Number: LMK05028 Other Parts Discussed in Thread: LMK00804B
We want to connect to VSC8512 PHY recoverd clock(125MHz) to PLL(LMK05028) Input which is LVCMOS, But according to the snippet attached LMK05028 Datasheet is saying that LVCMOS can take…
Part Number: LMK05028 Hi,
Let me ask you a question about the LOS\TCXO alarm as below.
As the LOS_TCXO status is in alarm state, I observed the waveform.
And I found the input waveform shown in the attached image.
- Voltage : 1.3V input
- frequency…
Part Number: LMK05028 Hi team,
I am working with the TICS pro and the LMK05028 with the following 2 register maps: Fs_40G_LMK05028.txt Fs_42G_LMK05028.txt
when im loading the register map i dont see any change on the first page:
saying that…
Part Number: LMK05028 Other Parts Discussed in Thread: LMK5B33216 , LMK5C33216A Tool/software: Hello,
We are using the LMK05028 in our design, and I am trying to simulate output delay using TICS Pro . However, I am not able to find any option for configuring…
Part Number: LMK05028 Tool/software: Hi,
We're using LMK05028 IC in circuit.
We're configured described hard pin mode in datasheet. In this case, the (ROM) LMK05028 output signals frequency is not shared in the datasheet.
What are the output signal…