Part Number: LMK05028 Hi Team
Is there a tool that we can use to control the device with GUI on PC through the I2C bus?
My customer wants to know if there's a connector to directly connect the SCK,SDA, and GND, and then connect another side (the dongle…
Hello Anji,
Unfortunately, I will not be able to support technical questions on software that is not our TICS Pro software. My recommendation is to either contact SMARTModular (a 3 rd party programming house) to assist with your device programming or program…
Part Number: LMK05028 Hi,
I would like to ask you a question about the parameter meaning of "DPLL Phase Lock Detectors".
Please tell me the meaning of following parameter set value.
- Lock Threshold
I am currently using the value "31" that…
Part Number: LMK05028
I had a few questions about frequency monitoring in reference input monitoring when I used LMK05028. The 8 outputs do not have a fixed phase difference with input clock (REF0). Until now, we find four status (PLL1 Lock Detected…
Part Number: LMK05028 Hi,
I also would like to ask you a question about DPLL Phase Lock Detectors as below.
Following my understanding is correct?
"The Lock ppm and Unlock ppm set here are deviations from the REF TDC Rate [Hz]."
For example…
Part Number: LMK05028
Hi team,
LMK05028 output configuration have to change as below sequence if I understand correctly.
1. Write 3fh to R51 : all output disable
2. Write to corresponding registers based on the updated configurations
3. Write 1b to R677…
Part Number: LMK05028 Hi There,
We are using LMK05028 device in our design and we are trying to program the chip through TICSPRO . (v1.7.5.4). Attached the .tcs file for reference. The programming successful and we are able to see the respective clocks…
Hello Kia,
Regional sales has called me. You can close this thread. After we get new PCBA, I may request LMK5B12204 configuration file from you.
Thanks again
Peter
Part Number: LMK05028 Hi,
My customer has been using TICS Pro to generate register setting of LMK05028.
When the customer executed "MATLAB Run Script" to generate register settings in TICS Pro ,
suddenly the message " The function or variable…
Hi Maoyuan,
I apologize for the extreme delay. I hope you've managed to resolve this issue.
maoyuan zhao said: I have confirmed that my REF0 is validated when I disabled the frequency detect. If I enable the frequency detect, REF0 is invalid and two…