Part Number: LMK1C1102 In the datasheet for the LMK1C1102, it says pins 5 and 7 are not connected (NC), and unused outputs can be left floating. Is it ok to gorund these pins instead?
Part Number: LMK1C1102 Looking for info on the thermal properties of LMK1C1102. Do you have the junction-to-case (Theta JC) and junction-to-board (Theta JB) values for this part in a bottom (board) cooled configuration? Thanks.
Part Number: LMK1C1102 Hi,
the datasheet of the LMK1C1102 specifies an output high voltage for the clock output of min. 0.8*V_DD. If supplied with 1.8V this means the output voltage is at least 1.44V for a high level. But there is no specification…
Part Number: LMK1C1102 I am looking at replacing an obsolete chip (from Analog Devices, LTC6957). I came across the LMK1C1102 that I think could work. We have a large variation in the amplitude of input waveform (Could be 10MHz Sine, Clipped-Sine, CMOS…
Part Number: LMK1C1102 Hi support team,
in our application: LMK1C1102 Y0 connect to SoC, Y1 via FPC to another system, this system have level shift with a pull up 1K resister to 1.8V, when this system power on, but our board still keep power off (without…
Part Number: LMK1C1102 Tool/software: Dear Sir/Madam,
I am looking at using the LMK1C1102 to buffer a crystal to a Cyclone 10 GX FPGA. The FPGA has banks powered from 1.8V and 3V. Typically the LMK1C1102 is powered from 3.3V and not 3V. What I want…
Part Number: LMK1C1102 Other Parts Discussed in Thread: TXU0102 Hi TI Team,
I am working on a design where I need to take a clock signal from a CPU and fan it out to a 1.8V UFS device. Here are the key interface specifications:
Clock Source (CPU…
Part Number: LMK1C1102 Other Parts Discussed in Thread: LSF0101 , LMK1C1108 , Output voltage of pin B1 and B2 are not changing to 3.3V. Default gets assigned to LSF0101_IO_5S but the voltages in Hyperlynx simulation is observed as 1.8V. When tried to…