Part Number: LMK1C1104 We have deployed design using LMK1C1104. We have observed the delay in clock output by some number of input clock cycles, which is causing some difficulties for our design.
Presumably, this is described by datasheet as t_start…
Part Number: LMK1C1104 Hi,
The datasheet listed supply voltage are 3.3 V, 2.5 V, or 1.8 V, my question is: Can I use 3V supply voltage and get additive jitter between 3.3V and 2.5V?
Regard!
Lee
Part Number: LMK1C1104 Hi,
Is the orange box in the figure below a Top View Pin Number layout ?
Does the R0.05 radius on the pins in the green box need to be modeled, or can they be created as rectangular pins ?
Are the Land Pattern…
Part Number: LMK1C1104 I’m considering using the LMK1C1104 powered at 1.8 V to accept a 3.3 V LVCMOS input clock and produce a 1.8 V LVCMOS output.
My understanding from the datasheet is that the inputs are 3.3 V tolerant at all supply voltages. Based…
Part Number: LMK1C1104-Q1 Hi TI Team,
Please confrom whether the PLMK1C1104QDQFRQ1 from LMK1C110x-Q1 is active in TI. Need a datasheet or please confrom active datasheet is www.ti.com/.../lmk1c1108-q1.pdf . But no product specific page for this part…
Part Number: LMK1C1104 What are the conditions for the test circuit in Figure 7-1?
How should I estimate the power supply current consumption when using a 50OHM load via a DC blocking capacitor as the output load? All 4CH TOTAL
Part Number: LMK1C1104
Hi,
I am reposting this because the original thread has not received any response, and there seems to be a bug preventing me from replying to that thread.
https://e2e.ti.com/support/clock-timing-group/clock-and-timing…
Part Number: LMK1C1104 Other Parts Discussed in Thread: LMV112 , CDC328A
Hi,
We are using four MCUs on a power controller board. Currently, each MCU has its own 8MHz crystal resonator, but we have an issue with clock frequency mismatch between the…