Part Number: LMK1D1204 Other Parts Discussed in Thread: LMK04832 Hi TI Team,
I am using the LMK1D1204 with a single-ended LVCMOS clock input. In my design, the LVCMOS signal is connected to IN− (N) and the bias voltage is applied to IN+ (P). The datasheet…
Part Number: LMK1D1204 Hi,
The datasheet for LMK1D1204 specifies when the IN_SEL input pin is left unconnected, the clock outputs are logic low. Does this mean that all OUT_P and OUT_N pins are driven to 0V, or does logic low in this case imply OUT_N…
Part Number: LMK1D1204 Hi,
I am considering to use LMK1D1204 as a buffer for a 0.8Vpp clipped sine generated from a VCXO:
How should I couple this signal to LMK1D1204? How should I bias both PRIREF_P and PRIREF_N?
Thanks,
Miguel
Part Number: LMK1D1204 Other Parts Discussed in Thread: LMK1C1104 Hi,
I have two LVCMOS18 clocks coming from an oscillator and an FPGA and i want to mux and drive LVCMOS18 output clocks to 4 camera sensors. How do i terminate the unused in_N and out_N…
Part Number: LMK1D1204 Tool/software: Hello team,
If the thermal pad of the LMK1D1204 is not connected to ground,
1) Is there a problem with the clock not being output or not being output correctly?
2) Does the LMK1D1204 reference the ground of…
Part Number: LMK1D1204 Tool/software: I am looking for a replacement for an Analog Devices Buffer/Driver part LT6957-4. This device has been used in my application to provide a high slew rate output from a sinusoidal 10MHz input. Low additive phase noise…
Part Number: LMK1D1208EVM Other Parts Discussed in Thread: LMX2592 , LMK1D1204 , LMK1D1208 , LMX2592EVM Hi,
I am using LMK1D1204 (Vcc = 3.3V) to convert a single-ended 10 MHz sine wave from a signal generator and produce four LVDS outputs that are fed…
Part Number: LMK1D1204 Tool/software: Hello,
I am using a single-ended LVCMOS clock with a 3.3V amplitude as the input. Please find the attached schematic for reference. I have a few questions regarding the biasing configuration.
Current Setup:…
Part Number: LMK1D1204 Other Parts Discussed in Thread: LMK6D Tool/software: Hello,
My customer requested a review from TI for their LMK1D1204 design below.
Please review the circuit design to see if there are any problems.
The output waveform…
Part Number: LMK1D1204
Tool/software:
Hi,
I am using LMK1D1204 IC in my design as below
SG3225's output clock is measured and seems to be ok.
But output clock of the LMK buffer seems to be non-monotonic and looks worser with diff probe…