Part Number: LMK5B12204 Other Parts Discussed in Thread: LMK5B33216 Hello,
I’m using an LMK5B12204 configured manually via I²C (no TICS Pro during runtime). I will attach my register configuration in the attachement.
Setup
SECREF is the prioritized…
Part Number: LMK5B12204 As shown in the figure, PREREF_P/N is input at 100 MHz, XO is also input at 100 MHz, and the two clocks are of the same source. I need to provide a continuous clock signal for the ADC to serve as the sampling clock. The frequency…
Part Number: LMK5B12204 Hi,
I have a question from my customer regarding the LMK5B12204;
Can I use the FINC and FDEC pins to change the phase? The datasheet suggests this is possible by enabling GPIO_FDEV_EN, but I can’t find GPIO_FDEV_EN in the register…
Part Number: LMK5B12204 Other Parts Discussed in Thread: LMK5B12212 , LMK5B33414 , LMK5B33216 Hi,
I know that the LMK5B12204 does not support ZDM, but if I can tolerate a deviation of about 2ns between the 10MHz input and the 40MHz output, can I reset…
Part Number: LMK5B12204 Other Parts Discussed in Thread: LMK3H0102 Tool/software: Hi,
My customer plan to DIN LMK5B12204 in their application, because we both do not have experience in using LMK5B12204.
Need your suggestions in the following design…
Part Number: LMK5B12204 Hello, I am sending the primary refrence (PPS) for correction and I can observe that Tunning History update interrupt is occurring periodically. But, as soon as i remove/disconnect my primary reference, the output is going to free…
Part Number: LMK5B12204 Hi , I wanted to write the register configs to EEPROM i was able to write and boot succesfully . But after 3 to 4 EEPROM writes the output clock had a constant frequency drift in all its outputs. I read the NVMCNT it was less than…
Part Number: LMK5B12204 Other Parts Discussed in Thread: LMK05318B , , LMK05318B-Q1 Tool/software: While testing LMK05318B and only needed 3 outputs, i was considering LMK5B12204.
The parts seems to be identical except for the output count. And pin…
Part Number: LMK5B12204 Other Parts Discussed in Thread: LMK05318B , AM6411 , LMK5B33216 , LMK05028 Hi Expert,
We have created a custom board using the LMK5B12204. After manufacturing several units, more than half of them take 3–4 hours to achieve frequency…