Part Number: LMK61E0M Other Parts Discussed in Thread: LMK01801 , LMK3H0102 Hi Tier
I found LMK61E0M which most suitable for customer need which is single-end output. programmable frequency. 100k-1Mhz output range.
But customer want to known do we have…
Part Number: LMK61E0M Hello,
I use a TICS Pro tool to program the LMK61E0M oscillator output frequency. I want to permanently store the programed value in the EEPROM, so the value will remain there after power cycle. Application store value only in the…
Part Number: LMK61E07 Other Parts Discussed in Thread: LMK61E0M , LMK61E2 Hello,
I am trying to validate if LMK61E07 can be used to generate 1 GHz CLK or not.
As far as I understood from the TICS Pro SW, it looks like 1 GHz CLK output is not possible …
Part Number: LMK61E0M Other Parts Discussed in Thread: USB2ANY , LMK6C , SN74LV4040A Hi team,
I am looking for programmable OSC and found that LMK61E0M might be a good option for me. I have a question on it and want to double check with you. In the datasheet…
Part Number: LMK61E0M Dear teams,
Nice to see you! I have a reference design for FPD-Link device and need an external oscillator LMK61E0M provided to REFCLK pin.
But I'm not sure that whether oscillator LMK61E0M s upport for ASIL system level or AEC_Q100…
Part Number: LMK61E0M Hi Team,
I used below setting to set LMK61E2M output frequency. (92Mhz and 184Mhz)
The 184MHz behavior looks good, but 92MHz is not ok. We tried 94MHz 90MHz and 91MHz, and the behavior were similar. Can you help me how to fix it…
Part Number: LMK61E0M Other Parts Discussed in Thread: LMK61E2 , Hi Team,
We are using this chipset to provide external clock to video unit for display.
I have checked but no Linux kernel driver is available.
Do you have linux kernel driver available for…
Part Number: LMK61E0M Hi Team,
We used LMK61E0M for oscillator. We would like to let output frequency equal to 185MHz and try to modify the R22/R23 register.
But there is no output when we done the register setting. May you let me know the correct flow…
Part Number: LMK61E2EVM Other Parts Discussed in Thread: LMK61E0M , LMK61E2 , LMK61E07 , LMK61E2-100M Hi Team,
I use TICS Pro V1.7.0.0 for LMK61E2EVM board and I select device -> osc -> LMK61E0M. (Use mini USB-J1 to connect)
But when I click the…