Part Number: LMX2594EVM Other Parts Discussed in Thread: LMK61PD0A2 , , LMX2594 Hallo,
I am intrested in the phase noise reachable with reference pro board (containing the LMK61PD0A2 Oscillator). Do you have any phase noise plots of the suggested setup in…
Hi Satya,
You can use a single output RFoutA instead of two outputs. If you are using single-ended terminate the unused side with a 50 ohm resistor. (Both RFoutA must be pulled up to Vcc)
If you are not using RFoutB, you can powerdown it down (by programming…
Other Parts Discussed in Thread: LMK61PD0A2 Hello,
Could you help check below part number is p2p to our LMK61XX-FFFMFF ? SiTime package size is 2.5 x 2.0 mm. not 7.0 mm x 5.0mm. Could LMK61XX-FFFMFF support 25MHz ?
SiTime OSC,25MHz,+/-25ppm…
Part Number: TICSPRO-SW Other Parts Discussed in Thread: LMX2595 , LMX2592
Hello, does anyone know how to initiate an output frequency sweep through the TICSPRO software. Looking to sweep an LMX2595 EVM across a range of frequencies with spacing of 1 kHz…
Part Number: LMX2572 Hi.
I have a problem with LMX2572 part.
When I program it for output with output frequency divider everything works ok - I see correct frequency and amplitude.(I program OUT_Force bit )
When I try to change output A multiplexer to…
Part Number: LMX2595 Other Parts Discussed in Thread: PLLATINUMSIM-SW Hello. I have few Queries regarding LMX2595.
1) It is clear that the output phase noise of LMX2595 mainly depends on how better the phase noise of the reference signal. Other than the…
Part Number: LMX2595EVM Hi pals!
I have some sort of a problem with Tics Pro. I'm trying to see logical changes of registers with my logic analyzer, I mean I can see which registers had written with TicsPro, but I want to see it with my logic analyzer…
Part Number: LMX2595EVM Other Parts Discussed in Thread: MSP430F5529 , , LMX2595 Hello sir, In the reference pro board of LMX2595EVM there is MSP430F5529 controller in reference pro board as I am about to make my own pcb.
1) May I know what exact pins …
Part Number: LMX2572EVM Other Parts Discussed in Thread: LMK61E2 , Test Setup LMX2572EVM with LMK61E2 MSP430 board using TICS PRO 1.6.10.0
Loading the default configuration for the EVM and trying to use the Fully Assisted VCO calibration, the locktime is…
Part Number: LMX2595EVM hello sir, I have few more doubts, kindly clarify
1) Even after loading in the default mode the PLL is not locking. The output is not stable at 7GHz but the lock detector LED is ON. For the frequencies upto 2GHz the output is…