Part Number: LMK62I0-100M Other Parts Discussed in Thread: LMK6H Hi Support
We would like to check if jitter specification of LMK62I0-100M could meet PCIe gen6 application. Please help to check.
Requirements :
1. package size: 5*3.2 mm
2. frequency…
Part Number: LMK62I0-100M Other Parts Discussed in Thread: LMK61E2EVM This question regards the OE pin on this device.
In page 3 of DS pin 1 is described:
"Outputenable(internalpullup).Whensettolow,outputpairisdisabledandsetathigh impedance."…
Part Number: LMK62I0-100M Dear TI Expert,
Forgive me if I am asking a stupid question. Why do we generally use phase jitter in between 12kHz and 20MHz (this specific freq range) as a parameter to evaluate clock's phase noise or jitter performance?…
Part Number: LMK62I0-100M Dear TI Experts,
We have a question about rework or resoldering chip of LMK62I0-100. We do see that this chip is of MSL3, which means its floor life at 30 degree C is 7days after opening drypack bag. If we suspect this compnent…
Part Number: LMK62I0-100M Dear team,
According to datasheet, LMK62i0 have internal pull high.
But we found we need to add external pull high to enable device output. Without external pull high, we cannot get clock output.
Could you help to confirm if…
Part Number: LMK62I0-100M Do you recommend a series resistor between the device and 50 ohm pull-down when driving HCSL inputs (PCIe)?
If so, what value?
Thanks
David
Other Parts Discussed in Thread: LMK62I0-100M , LMK6H Hi team
We have PCIE GEN 5 in our system , for REF CLK M / P can we use this part LMK62I0-100M00SIAT ? I saw most of specs are meeting but if any one confirms this part will support REF CLK of GEN 5