Part Number: LMKDB1104 Other Parts Discussed in Thread: LMKDB1108FS hi sir
we would like to replace RC19004 By LMKDB1104
some issue need be clarity as below
Q1:What is the different of LMKDB1104 & LMKDB1104FS
Q2:IN/Output frequent support the…
Part Number: LMKDB1104 Hi team,
We got some question about the datasheet, please kindly share some input.
What does the meaning of SLEWRATE_SEL_CLK2_MSB? Default is 1, what happen if set to 0?
Does our device support saving config in the device…
Part Number: LMKDB1104 Hi team,
My customer has encountered an issue that our clock buffer is faster than DS listed.
We tried pin mode that can lower the slew rate, but PCIE spec is 4V/ns,
SLEWRATE_SEL = High: Slew Rate is 4.7–4.8 V/ns
SLEWRATE_SEL…
Part Number: LMKDB1104 Hello,
in our design we use LMKDB1104.
we use LVDS clock, use AC couple 10nF and use 100Ohm termination P to N.
we don't change RX_EN_AC_INPUT register value. default is '0' meaning DC couple.
does this design is not according…
Part Number: LMKDB1104 Hi Team,
Can I know which typical applications use 100ohm differential impedance and which applications use 85ohm differential impedance?
Regards, Hailiang
Part Number: LMKDB1104 Other Parts Discussed in Thread: LMKDB1102 Tool/software: Dears,
My client is looking for a clock buffer for PCI express to SATA/SSD conversion. The input is the server motherboard clock, and the output type is HCSL with 2 outputs…
Part Number: LMKDB1104 Tool/software: Hi Expert,
Customers want to know if PWRGD/PWRDN# can be directly connected to a high level? They do not need the PG function. If it cannot be directly connected to a high level, how long is it recommended to pull…
Part Number: LMKDB1104 Tool/software: I am look for a 1 to 4 PCIE Gen4 clock buffer/fanout, 2 clocks to PCIe add-in card and 2 clocks to AMD FPGA GTY transceiver reference clock
Looking for a simple buffer that do not need much setup, maybe a pin to…
Part Number: LMKDB1104EVM Other Parts Discussed in Thread: LMKDB1104 , LMKDB1204 Tool/software: When can I apply for sample testing for LMKDB1104 and when can I start mass production?
Whether to provide a specific description of REY(VQFN,20) package…
Part Number: LMKDB1108EVM Other Parts Discussed in Thread: LMKDB1108 , LMKDB1104 ,
Dear Customer Support,
The LMKDB1108 EVM User's Guide describes 16 programmable output slew rate settings (SLEWRATE_OPT1~4).
However, in…