Part Number: LMP2011 Other Parts Discussed in Thread: TINA-TI Tool/software: Hello,
When using the LMP2011 PSpice model (Rev C., snom113c..zip), PSpice encounters convergence issues when trying to calculate the model's bias point. Initial bias point…
Part Number: LMP2011 I have created a simple non inverting voltage follower with input voltage DC offset of 1.25 V and a peak amplitude of 1 V. However, the output clips off at close to 1.65 V. The supply to the IC is single supply 3.3 V. I have attached…
Part Number: LMP2011 Other Parts Discussed in Thread: TINA-TI , OPA335 , , LMP2012 I am trying to run noise analysis on this part, but have repeatedly run into an error message: "Access violation at address 00874877 in module 'TINA.EXE'. Read of address…
Part Number: LMP2011 Hello,
I want to implement the circuit shown in the attached application note (wonderfully explained, by the way), to measure a 4 wire RTD.
I have two questions:
1.- Is C1 capacitor value of 1F correct? It seems too big, and LMP2011…
Part Number: THS4561 Other Parts Discussed in Thread: LMP2011 , OPA2994 , LM7332 , TLV2333 , OPA4354 , INA826 , OPA2810 Hi team,
For our project we are using load cell. For amplifying the load cell output, the THS4561 amplifier circuit is used.
Refer the connection…
Part Number: LMP2011 Hi team,
My customer has a issue in their system when using LMP2011, the output current is not stable ,please help to check the sch if the setting of parameter is not right?
Other Parts Discussed in Thread: LMP2011 , INA114 , OPA376 , LMP7721 , LMP7701 , OPA277 , OPA192 Hi,
I'm designing a voltage-to-current converter (e.g. based on Figure 13 in the INA114 datasheet), trying to achieve 100pA accuracy, so I need an op-amp with low…
Other Parts Discussed in Thread: TL061 , LMP2011 , TL072 , LMP2021 Hi,
My customer needs the following information.
Could you show me the input--referred current noise of LMP2011 & TL061?
Thanks and Regards,
Kuramochi / Japan disty
Other Parts Discussed in Thread: LMP2011 , TINA-TI , LMP2021 Hi all,
Is there anybody who can help provide me the parameters of ' Input Common-Mode Voltage Range‘ under 5V supply voltage for LMP2011 ? When i simulation it with TINA-TI, Flat-top …