Part Number: LMP2231 I have a high gain circuit that oscillates, to calculate Cf, the input capacitance of the op amp would help greatly, it isn't on the datasheet.
Part Number: LMP2231 Here's how I described this situation in a case that I opened a few days ago. The engineer who responded could not answer this question.
Short description: How to avoid electrical overstress of input during power-down of lmp2…
Part Number: LMP2231 Other Parts Discussed in Thread: INA826 My input voltage range is: +/- 500mV.
Output voltage range: 0 to 2.5V which is driven to ADC.
Supply voltage available : +/- 2.5V.
I would like to know how can i design this circuit and also…
Part Number: LMP2232 Other Parts Discussed in Thread: OPA2196 , LMP2231 I has asked about alternates for an LT2078CS8 and the LMP2232 was suggested, but the max supply voltage is shown as 6V.
Safe to assume that +5V and -5V rails would be out of spec? …
Part Number: RF430FRL152H Other Parts Discussed in Thread: LMP2231 , Hi,
I want to know why the amplifier(U1 LMP2231) was used at sensor components which consist of a galvanic skin response(GSR) sensor and a thermistor.
I've designed a GSR sensor usi…
Part Number: LM2904 Other Parts Discussed in Thread: PSPICE-FOR-TI , , LMP2231 My customer said: In a PSPICE-FOR-TI there is model, but it can it cannot be put on the schematic.
Can you please check what could be an issue.
Thanks
Viktorija
Part Number: LMP7721 Other Parts Discussed in Thread: ADS1246 , LMC6482 , , LMP2231 Dears
I want to choose a 24bit, I/V conversion pre-op amplifier for the silicon photovoltaic cell, the photocurrent is 40pA~500nA , and the low input offset current LMP7721MAX…
Hi Nestor,
Usually, chopper op amp datasheet indicate when that is the case. I reviewed the details of the datasheet for the LMP2231/LMP2232 and LMP2234, and there is nothing in the specifications that would indicate that it is a chopper design.
For…
Hello Akaba-san,
I apologize, I do not think I fully understood the question and my previous response was not very clear. I should have provided additional information.
The ADS1298R does not have a peripheral to support GSR on it's own.
From…