Other Parts Discussed in Thread: LMP8603 Dear, Sir.
LMP8603 has "OFFSET" pin for bidirectional current sensing.
The output is 1/2 voltage applying the "OFFSET" is referenced to mid-rail voltage.
The datasheet indicates "OFFSET" pin tied to "VS"…
Hello,
Please answer question about Total Gain Error and Input Offset Voltage.
Total Gain Error(9.95V min/ 10.5V max) and Input Offset Voltage(+-1mV max) are specified under V S = 5V, −22V ≤ V CM ≤ 60V and Sense Voltage(+IN - -IN) is not specified…
Part Number: INA237-Q1 Other Parts Discussed in Thread: LMP8603-Q1 , INA148-Q1
hello, for automotive efuse with high-side current sense under reverse polarity condition, i anticipate that input protection diodes on in+/in- , even if supply is protected…
Part Number: LMP8601 Other Parts Discussed in Thread: LMP8603
Hi Colleagues,
Hope all is well over there, where sun always shines :-)
I have a customer evaluating the LMP8603 and was wondering if we have data to plot the common mode voltage versus…
Other Parts Discussed in Thread: LMP8602 , LMP8603 Hi,
We want to use LMP8602 as a Shunt monitor over a active Shunt (MosFET). The supply of the LMP8602 is 5V.
We have a differential input voltage of 16V max. in fault condition. I didn't find any…
Other Parts Discussed in Thread: LMP8603 Hello,
Figure 3 on the LMP8603 data sheet (SNOSB36D) shows the change in V_offset as a function of the common mode input voltage and the chip temperature. For a given chip, how repeatable are these curves, and…
Hi Vincenzo,
Thank you for providing additional details.
If you give me a few days I can order and test this device on the lab, but please have in note, the obtained values may differ slightly in other production devices.
Most of our newer devices…
Part Number: LMP8602 Hi Team,
Good day !
We have received attached PCN: 20260706000.1 notice found one more part of same series in Keysight database. Would like to confirm with you, if MPN: LMP8602MMX/NOPB is impacted by this PCN Notice or not.
…
Hi,
wayne lu1 said:
Although I still need to use power line to transmit the data about the motor's speed or something else to control the motor.
So, do I need to buy a new device or any software I can use?
if you wish implement motor control…