Part Number: LMQ644A2-Q1 Hi Team
Our product incorporates the LMQ644A2-Q1 IC for 3.3V@12A and 1.8V@12A
The configuration parameters are outlined below:
- Input Voltage (Vin): 11 to 13V and 12V nominl - Output Voltage / Output Current (Vout/Iout…
Part Number: LMQ644A2-Q1 Other Parts Discussed in Thread: LMG708B0 We have confirmed that LT8648SEV#PBF is currently unavailable with a long lead time.
Therefore , we would like to ask if you could recommend alternative parts.
Input voltage :about…
Part Number: LMQ644A2-Q1 Tool/software: Dear TI Support Team,
I found a design using the LMQ644A2-Q1 dual buck converter with 3.3V and 3.8V outputs, which matches my requirements. Could you please share the Altium schematic and layout source files for…
Part Number: LMQ644A2-Q1 I tried to model this component in Webench:
Output Type: Single, dual-phase
Input : 9 - 16V
Output : 12A max @ 3.3V
1.) The resulting schematic shows FB1 being left open. Why is not being tied to ground, as per data…
Part Number: LMQ644A2-Q1 Other Parts Discussed in Thread: LMQ644A2QEVM-D2100 Tool/software: WBDesign15 (1).pdf
I plan to utilize the LMQ644A2-Q1 integrated circuit for a specific solution. Below are the details: My system operates on 24VDC, and to…
Part Number: LMQ644A2-Q1 Tool/software: Dear Support Team,
We are currently designing a new project utilizing the LMQ644A2-Q1 in single-output mode as our primary power supply. During certain operational scenarios, the input of the LMQ644A2-Q1 may be…
Part Number: TPS546D24A Other Parts Discussed in Thread: TPS543C20 , LMQ644A2-Q1 , LM3880 , TPS386000 , TPSM5D1806 Hello TI Team,
I am designing a power supply and sequencing solution for an Intel/Altera Agilex 5 SoC and would like to verify the suitability…
Part Number: LMQ644A2-Q1 Dear Team, Please find the attached image
In the above attached image, could you please explain what is Interleave?> Since in WEbench power designer, When i am Searching for the Above part there are more options as in the below…
Part Number: LMQ644A2-Q1 Tool/software: Hello everyone,
I'm working on designing a PCB using the LMQ644A2-Q1 step-down converter to get a 12V output at 12A from a 28V DC input. I based my design on the LMQ644A2 Quickstart Tool I previously used for…
Part Number: LMQ644A2-Q1 Tool/software: Hi Team, Can you please review the schematic for 16V,4A output with input voltage range from 18V to 24V? Thanks, Gaurav Ingle