Part Number: LMV331 Team,
Customer is asking why LMV331IDCKR device marking was R2F only in the past, but later came with others like R2C/R2I, and eventually become R2F/R2K/R2R now.
Part Number: LMV331 hello
Pls check and advie if there are Large reel packaging size PNs for the below items . If yes, pls advie the related part information
tks
Current
New
Part
MPN
MOQ
MPQ
Large packing MPN
SPQ
MOQ…
Part Number: LMV331-Q1 Hi expert,
We want to know the device temperature grade of LMV331-Q1, I can't find the information in datasheet.
below is a example of other device:
Part Number: LMV331-Q1 Dear TI experts,
Could you check the ESD (HBM,CDM) specification of LMV331QDBVRQ1?
I cannot find it in the datasheet.
Best regards,
Chase
Part Number: LMV331 Other Parts Discussed in Thread: LMV339 Hello TI team,
The customer is using LMV331IDBVR
Please assist in providing the following
Junction-to-case (top) thermal resistance
Junction-to-board thermal resistance
Thanks
Part Number: LMV331 Other Parts Discussed in Thread: TLV9020
Tool/software:
Hi Ti team
I designed a Hysteresis circuit using LMV331 to power off at high temperature and turn it back on when the temperature drops.
However, the Output swings before…
Part Number: LMV331 Tool/software: Hi TI Team,
When the customer was looking at the LMV331 specification, there were some sentences underlined in red as shown in the following picture that they did not understand. Please help explain them. Thank you…
Part Number: LMV331 Other Parts Discussed in Thread: TLV9020 , ALL HI.
As shown in the following picture. The chip specification is the description of the input common mode voltage, the maximum input common mode voltage can not exceed vc-0.7v, beyond…
Part Number: LMV331 Other Parts Discussed in Thread: LM339 Tool/software: Hello,
Could you clarify, if valid output is guaranteed over temperature for below input and VCC conditions of LMV331.
Device: LMV331I
Vcc+ to GND: 3.2V
IN+ input 4.2V …
Part Number: LMV331 Tool/software: Hi team,
please help me take a look at this schematic from customer,
since LMV331 doesn't have POR,
As you can see both the IN+ and IN- are divider of same 5V from VCC, does this VCC power up situation match exactly…