Part Number: LMV339 Hi team.
I am confusing about absolute maximum ratings.
I'd like to give me your advice in below things.
1. The minimum of VICR(-0.1V) exceeds the absolute maximum rating(VI=0V).
Why is this?
2. If it is mistake , will…
Sorry for the confusing information in the datasheet. We will need to investigate and respond to you early next week. We are on holiday break for the rest of this week.
Chuck
Part Number: LMV339 Other Parts Discussed in Thread: LMV331 , TLV7032 , TLV7042 VICR Common-mode input voltage range is only specified at 25°C
What is the performance for VICR Common-mode input over full operating temperature
Part Number: LMV339 Hello support team,
Is there a clamp diode (between VCC and GND) for ESD protection at the input pins (IN +, IN-) of the LMV339? If so, what is the value of Vf of the diode? Also, is there anything that allows comparator inputs to…
1. the transient analysis was taking long time for a long duration analysis
2. i dont know why my circuit having a 3 to 4 stages of opamps is making the output to appear after a delay, why ?
3. as soon as i run the simulation its default dc and shifting…
Other Parts Discussed in Thread: LMV339 Hello,
My customer uses the LMV339, an input signal is applied when the LMV339 supply voltage is zero.
The input current is less than 1mA and the input applied time is less than 20msec.
Is this condition OK…
David,
The LMV339 has the legacy TI die and the LMV339-N has the legacy National die. Both devices will have similar performance when used in the allowed range.
Part Number: LMV331 Other Parts Discussed in Thread: LMV339 Hello TI team,
The customer is using LMV331IDBVR
Please assist in providing the following
Junction-to-case (top) thermal resistance
Junction-to-board thermal resistance
Thanks
Part Number: LM339 Other Parts Discussed in Thread: LMV339 , , TLV1702 , LM393B , TLV9024 , LM2903B , TLV7044 Hey!
Are there any comparators similar to the LM339 which come in a QFN package? I did an unfruitful parametric search (likely because I…