Other Parts Discussed in Thread: LMV722 Hi,
Does anyone have the data of LMV722 output voltage Swing for the condition below,
VCC+=5V, VCC-=GND, RL=1KΩ to VCC+/2, full temp range
We'd like to know the amximum voltage for VOL.
Thanks
Go
Micheal,
The only reason this worked for seven years, is because the application depends on two flaws of LMV358. LMV358 had phase inversion for pin 5 below (more negative than) about -550mV. This phase inversion makes output high. The second flaw was…
Hi Thomas and Kai,
To add more possible low cost devices (CM to ground, < 22nV/RtHz noise, > 1MHz, 20mA output current, dual), here they are:
Device
RR Out?
CM to ground?
Cost (1k units) $
LMC6032
Yes
Yes
0.35
LMV722
Yes
Yes
0.39
TL34…
Wiky,
9nV may be from simulation, from characterization samples, or just copied from LMV722-N data sheet.
11nV came from a sample that may not be from original char samples.
Not every device will have the same voltage. Some will be a little higher or…
Other Parts Discussed in Thread: DRV8833 , LMV722 Hi
I need to measure the current sensing for Hdridge driver, in my design iam using DRV8833, the Hbridge driver have current sensing pin. so iam using current sense amplifier to measure the current.
please…