Other Parts Discussed in Thread: LMV761
Below is the schematic in customer's application system. "IN" is the input for a 1MHz signal.
When a 1MHz signal is applied on the "IN" in the front of C4. a same frequency signal i…
Other Parts Discussed in Thread: LMV761 need to get the spice model for LMV761 to run properly in LtSpice---it has several syntax errors, and I am not and expert of fixing such errors. I must have a PCB completed in the next several days, and I must simulate…
Other Parts Discussed in Thread: LMV761 Is the LMV761 similar to other TI/National Comparators in that just one of the inputs need to be within the common mode range in order for the outputs to behave as expected?
Part Number: OPA333 Other Parts Discussed in Thread: LMV761 , OPA391 , OPA369 Hi TI experts,
We are trying to use below circuit to detect the ASIC version, depending on the HBM_SNS pin status. Can you please review below circuit and check if below function…
Hello Andy,
At these speeds, they need to use a "real" comparator.
The functionally closest would be the TLV3501, though it is not P2P. Offset is a bit more because the temperature range is wider (125C).
The closest P2P compatible would…
Hello Del,
See page 13 of the LMV761 datasheet: www.ti.com/lit/ds/symlink/lmv761.pdf . The LMV-series is low power, hopefully the frequency you need can be generated with this simple circuit.
~Leonard
Part Number: LMV762Q-Q1 Other Parts Discussed in Thread: ISO7721 , LMV762 , LM311 Hai Paul Grohe,
Thanks for your clarification on the matter. Subjected to this query,please see the attached SiC Mosfet gate driver design of TI.
TI Designs: TIDA-01605…
Other Parts Discussed in Thread: LMV762 Hello,
I am planning on using the LMV762 for a line fault detection circuit.
One comparator for line break, one for short circuit detection. When e.g. a line break occurs, the short circuit comparator will see a…