Part Number: LMV772-Q1 Tool/software: Hi
Please provide LMV772QMMX/NOPB (5 pins) Safety manual for this and also Pin FMEA/DFMEA.
Thanks
Regards,
Lakshmishree B P
Part Number: LMV772-Q1 Other Parts Discussed in Thread: LMV772 Tool/software: I am using the opamp LMV772.
I have non-Inverting negative feedback opamp configuration with gain is 11.
The opamp I/P is connected to a voltage divider and the application…
Part Number: LMV772-Q1 Other Parts Discussed in Thread: LMV772 Hi
I used a TI op amp lmv772 in the application. Now I want to calculate the error caused by the op amp.
Could you please help to check out the input offset and what other parameters can…
Part Number: LMV772-Q1 Other Parts Discussed in Thread: LMV772 Hello,
I am using a dual channel LMV772. Presently I need only one channel for my application. What is the method to diable the other Op-Amp in the device? Is it better to ground it or leave…
Other Parts Discussed in Thread: LMV772-Q1 Dear all,
I would like to know about temperature drift.
LMV772-Q1 has two OpAmps in one IC.
Do these two OpAmps have same temperature drift?
Do these two OpAmps have same error of temperature drift…
Only the "MAX" values in the datasheet are guaranteed.
The TLV9062-Q1 is a low-cost device. There is no exact replacement for the RS722P. Other low-cost devices would be OPA2377-Q1 or LMV772-Q1; devices with similar or better characteristics in the…
Part Number: LMV772 Other Parts Discussed in Thread: TLV3501A-Q1 Tool/software: Please provide aFMEDA ,DFME and safety document for the below component 1.LMV772QMMX/NOPB
2.TLV3502AQDCNRQ1
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…