Part Number: LMV981-N
This is Bhuvaneswaran B from Flex, currently we are working with one of our manufacturing plants, to collect the Shelf Life for all the active components.
Since we are unable to identify the Shelf Life for the below Mentioned…
Part Number: LMV981-N Other Parts Discussed in Thread: LM358 Hi team,
My customer designed this device and met application problem need BU's support. Thanks
1. When the input voltage of LMV981_+IN is below 20mv, the response time of output LMV981_OUT…
Part Number: LMV981-N Other Parts Discussed in Thread: TLV9001 Our customer need LMV981MFX ESD CDM level and CDM test standard ,AND latch current paremeter
I don't see the parameters in datasheet, where can I get the parameters or reference , thanks…
Part Number: LMV981-N I have the datasheet revision M. The GBW is specified as 1.4 MHz but all the gain charts seems around a 10-fold lower. In Figures 6, 7, 8 and 9, no one show a zero dB gain over 1Mhz. It is more ranging from 400 kHz to 800 kHz. Since…
to User473,
I searched all the op amp portfolio with the parametric search (precision, general purpose, and high-speed). There are 6 options with temperatures of 150C and above (see attached). The best match is the OPA211-HT (210C max). This is the…