Part Number: LMX1204 Other Parts Discussed in Thread: LMX1906-SP , Tool/software: Hello, My customer has three questions about LMX1204 and LMX1906-SP. Please respond those questions. Questions about LMX1204 and LMX1906.docx Best regards, K.Hirano
Part Number: LMX1204 Hi All,
I have a question regarding the LMX1204EVM.
Could you please tell me the part numbers for L6 and L7 listed below? They were not listed in the parts list.
www.ti.com/.../snau266a.pdf
Best Regards, Ishiwata
Part Number: LMX1204 Tool/software: Hi,
I need to sync multiple LMX1204 across multiple boards.
Each borad ( LMX1204) has a 6GHz input clk & sysref_req input.
Each LMX ouputs:
clkout = clkin/4 = 6/4 = 1.5GHz
sysref_out = clkin/6000 = 1MHz…
Part Number: LMX1204 Tool/software: I want to generate 3 different clocks from a single clk_in reference
CLK_in = 10GHz
1 output on 5GHz (clkout0)
1 output on 156.25 MHz (logisys)
3 outputs on 15.625 MHz (sysrefout)
how do set this up? I am…
Part Number: LMK04828 Other Parts Discussed in Thread: LMX1204 , DAC39RF12EVM , DAC39RF10EVM
Hello,
This is another post on a series related some issues we have correctly programming an LMK04828B and a LMX1204 on some eval boards and we would like…
Part Number: LMX1204 Tool/software: We want a fixed phase relationship between CLKOUT and SYSREF generated by LMX1204. When using LMX1204 for clock and sysref synchronization, the phase cannot be fixed.
Four SYSREFOUT, one LOGICLKOUT and one LOGISYSREFOUT…
Part Number: LMX1204 Tool/software: LMX1204 output LOGICLKOUT(logic clock) failure issue.
Below is my design. Pin 2/3 is float. I want to output the LOGICLKOUT on pin 27/28. After I configure the LOGIC_EN (R8 register) and LOGICLKOUT_EN(R8 register…
Part Number: LMX1204 Other Parts Discussed in Thread: LMX2820 Tool/software: Dear Specialists,
My customer is considering LMX1204 and LM2820 for JESD204B CLK.
They have questions, I would be grateful if you could advise.
---
We have questions…
Part Number: LMX1204 Tool/software: Hi team,
i chose the LMX1204 for clocks and sysref distribution for a new hardware project.
From the datasheet, the sysref output are differential CML, but i could use this the sysref outputs in single-ended mode…
Part Number: LMX1204 Tool/software: Dear TI Engineer,
We need an RF mixer with an IF/RF frequency range of 1-4.5GHz, and the LO frequency band is between 1-3GHz. Do you have any recommendations for this requirement?
Thanks,
Kind Regards