Part Number: LMX1205 Other Parts Discussed in Thread: LMX1204
Hi team,
For the LMX1205, is a VCM biasing circuit required on the SYSREFREQ pin?
For comparison, the LMX1204 datasheet recommends a SYSREFREQ input circuit that biases the signal…
Part Number: LMX1205 When using your company's LMX1205, the reference input is set to 10GHz. The frequency division generates 2.5GHz, 250MHz and 100MHz. Currently, the 2.5GHz output is normal, but the 250MHz and 100MHz outputs are not working properly…
Part Number: LMX1205 Other Parts Discussed in Thread: LMX1204
Hi team,
I have several questions regarding the LMX1205 input biasing recommendations.
Q1: About SYSREFREQ_VCM (Table 6-15 in the LMX1205 datasheet)
My understanding is that SYSREFREQ_VCM…
Part Number: LMX1205
Hi,
Do you have any data or graphs showing the dependence of LMX1205 output power on temperature?
The datasheet does not appear to provide any specifications or curves related to this parameter. However, based on my own measurements…
Part Number: LMX1205
Hi,
Currently we are using LMX1205 as a Clock buffer. Having some queries related to that,
1) Input sensitivity given as 0 to 10dBm for single ended input, What will be Input voltage swing for the differential input?
2) does…
Part Number: LMX1205 Hi team,
i'm using the IBIS model of the LMX1205. I try to simulate the CLKOUT model: i selected the pin 18 and 19.
I attach the electrical schematic.
The port number 3 is the signal source (square wave with frequency…
Part Number: LMX1205 Hi,
i need to use the LMX1205 with single-ended input. I read from the datasheet (figure 6-2) that, for optimal device performance, a voltage offset between the CLKINP and CLKINN required.
In the evaluation board this external…
Part Number: LMX1205 Other Parts Discussed in Thread: USB2ANY Tool/software: Hello TI team,
I’m currently using LMX1205 with TICS Pro and a USB2ANY adapter . Using the GUI works fine, but I need to programmatically control the LMX1205 registers (read…
Part Number: LMX1205 Other Parts Discussed in Thread: USB2ANY , LMX2594 Tool/software: Hello TI team,
I’m currently using LMX1205 with TICS Pro and a USB2ANY adapter . Using the GUI works fine, but I need to programmatically control the LMX1205 registers…
Part Number: LMX1205 Other Parts Discussed in Thread: TICSPRO-SW Hi Team,
Could you please advise how I can resolve the following issue?
When I tried to download the latest version of TICSPRO-SW (Version 1.7.10.1, released on Oct 17, 2025), the following…