Other Parts Discussed in Thread: USB2ANY , LMX2430 , USB2ANY-UWIRE Hello, Our customer would like to evaluate LMX2430EVM by USB2ANY. Since they don't have the USB2ANY , I will provide USB2ANY to the customer. However, I don't have the Adapter board..…
I tried the following:
1- Open Pllatinum Sim and select device LMX2430 --> "Load Device"
2- Save design
3- Close and reopen Pllatinum Sim
4- Select device LMX2492 --> "Load Device"
5- Load design previously saved
Result --> Unhandled exception:…
Mathieu,
The LMK4100 series can handle the 1 kHz input frequency and generate your output frequency, but is much higher than 5 mA.
We have LMX series PLLs that are below 5 mA (LMX2430), but can't handle 1 kHz input or go down to 16 MHz. I couldn't…
Moki,
All the LMX series of PLLs, which is the series that I am familar with, use a phase frequency detector, that will track the frequency, even if the phase is off. Consider the LMX2485 or LMX2430 series of integer PLLs. Hopefully, these are not too…
Satosih-san,
Indeed this is a different VCO. We have a serious problem with VCO vendors obseleting VCOs or VCOs not being available, so we switched to these crystek VCOs that are available on digikey. The correct BOM is as follows:
LMX2434…