Part Number: LMX2434 Hi,
Based on the data sheet, the last line of marking for LMX2434TMX/NOPB is "TMD", but the parts we ordered are with the marking "TMC".
Could you help to check the reason for the difference?
Thank you.
Other Parts Discussed in Thread: LMX2434 , LMX2492 Hello
I'm Alber as a FAE in Arrow Korea.
My customer asked about LMX2434 CPout voltage.
They usually use the 5V VCXO to use widely frequency range that Voltage Control range is 0V to 5V.
But…
Hi Dean-san,
This business is in under development phase so it's possible for cancel, but they bought two LMX2434EVALs to evaluate 4.8GHz VCO frequency because the user's guide state that it can be used with 4.8GHz. So I would like you to obtain and…
Other Parts Discussed in Thread: LMX2434
We have procured the Evaluation boards for LMX2434, and I'm satisfied that it is working as per the specifications of the RF PLL loop, But I could not verify the IF PLL, as there was no VCXO ('U3' as per the…
Other Parts Discussed in Thread: LMX2434 Dear Sir \ Madam
In my design I need to phase compare 2 high frequency signals (2GHz).
I think of using the LMX2434 phase detector part and the divider part as follow :
the first signal go from the signal…
Hi Sapir,
The LMX2434 EVM was design many years ago, the pin assignment of the socket is very different from USB2ANY.
shown below is the pin assignment of USB2ANY, I am afraid you have to manually wire the pins to the EVM accordingly. Please also…
Ryuji,
I have windows 7 and was able to simulate this with the clock design tool and change the parameters. But if you are having issues, try another device like the LMX2433 or lMX2434, which are from the same family, or try the custom PLL. Have you…