Part Number: LMX2572LP Other Parts Discussed in Thread: LMX2572 Just a preliminary question trying to select the right part.
We have a requirement to FM (modulate) a 100-500MHz carrier using a 20-20kHz analog audio input. The audio is passed through…
Part Number: LMX2572LP I'm considering reducing the current.
The current settings are as follows: 1. RFout = 1500~1600MHz 2. REF = 32MHz 3. Output level = -3 dBm typ. 4. total current = 80mA typ.
I'd like to explore whether the current can be reduced…
Part Number: LMX2572LP Other Parts Discussed in Thread: LMX2594 , LMX2572 Tool/software: There are spurs I observe which isn’t predicted by PLLatinum Sim There are some spurs that I couldn't find the root causes. I simulated on PLLatinum Sim, I used same…
Part Number: LMX2572LP Hello,
I wanted to confirm that the LMX2572LP RF outputs can be routed as a tightly coupled 100 ohm diff pair to drive a differential input clock.
Thanks
Joe
Part Number: LMX2572LP Other Parts Discussed in Thread: LMX2572 Hi,
We use LMX2572 in full‑assist mode with MUXout = lock detect. We hop through N frequencies (e.g., N=201). We always wait for LD high before starting the next hop. Normally we capture…
Part Number: LMX2572LP Tool/software: Thank you for your previous answer. I have some more:
1. Regarding your previous answer, do you think that combined the signals from both ports using short wires (A+ to B+, A- to B-) allows me to cheaply get extra…
Part Number: LMX2572LP
Hi,
I would like to confirm the correct settings for PFD_DLY_SEL and MASH_ORDER when using the LMX2572LP at the following output frequency.
We would like to generate:
RFout = 835.950 MHz
Channel divider = 4
VCO frequency…
Part Number: LMX2572LP
Hi,
I would like to confirm the correct settings for PFD_DLY_SEL and MASH_ORDER when using the LMX2572LP at the following output frequency.
We would like to generate:
RFout = 835.950 MHz
Channel divider = 4
VCO frequency…
Part Number: LMX2572LP Other Parts Discussed in Thread: LMX2572 Hi there,
We are currently using the LMX2572 as a PLL in a direct conversion transceiver. We are trying to use this in a "frequency hopping mode". To do this we are using the fully assisted…
Part Number: LMX2572LP Other Parts Discussed in Thread: LMX2491 Tool/software: whether the LMX2572LP can generate a linear sweep signal with a 40ms sweep period over the 650M-750M frequency range?