Part Number: LMX2581 We are trying to implement FM on a 450MHz output signal. which we get an response ,( AM implement on loop filter)
but this is not stable or consistant over our Audio frequency range ( 1-40KHz)
Do you think this is possible to…
Part Number: LMX2581 Hi there,
After recently creating my own board for the LMX2581, I am getting terrible spurs at Fosc offset. Using a 50MHz crystal, seeing spurs at 50, 100, 150 MHz away at -40dB down from main wanted signal.
Any idea on how to…
Part Number: LMX2581 Hi, I was given a certain project to lead. It was carried out by a person who is no longer with us and I have a problem finishing it. On the developed board there are 2 pieces of LMX2581. I managed to run the power supply (stable…
Part Number: LMX2581 Other Parts Discussed in Thread: , LMX2572LP I need some advice regarding the LMX2581.
Fosc: 10MHz, Fout: 280MHz, Fpd: 10MHz. As a result of actual measurement, spurious at intervals of 10 MHz is observed at 280 MHz. This spurious…
Part Number: LMX2581 Data sheet on Page 7 says OSCIn input voltage min=0.4Vpp, max=1.7Vpp.
Figure 12 and 13 show a much lower sensitivity, on the order of -27dBm.
Can you explain the differences in the data sheet?
Also, I'm using a CMOS TCXO and…
Part Number: LMX2581 Please give me some advice regarding the MUXout (LD) of the LMX2581.
OSCin:120MHz, RFout:1540MHz. The setting of LMX2581 is as follows, and data is written from R5(int). Even if OSCin is turned on from off, MUXout remains High Level…
Part Number: LMX2581EVM Other Parts Discussed in Thread: LMX2581 Request review materials for product design.
LMX2581 Evb Design Source.
Ideally gerber files and, if possible, a step 3D of the board.
Thanks
Part Number: LMX2581 Other Parts Discussed in Thread: CODELOADER , HI,
i am finding the setup file of CODELOADER 4,but i just find a "snac014.workz" on the TI.COM. SO ,pls SEND ME A LINK TO DOWNLOAD THE WHOLE CODELOADER SOFTWARE,THANKS!