Part Number: LMX2581 Other Parts Discussed in Thread: LMK04906 , , CODELOADER , USB2ANY Hi.
In project we have using two LMX2581 in one PCB, both are the the same circut, role, and very similar layout. On the other hand, layout doesn't differ significantly…
Part Number: LMX2581 Other Parts Discussed in Thread: CODELOADER , HI,
i am finding the setup file of CODELOADER 4,but i just find a "snac014.workz" on the TI.COM. SO ,pls SEND ME A LINK TO DOWNLOAD THE WHOLE CODELOADER SOFTWARE,THANKS!
Part Number: LMX2581 Other Parts Discussed in Thread: PLLATINUMSIM-SW Hi
when I read LMX2581 datasheet, I am confuse about Dithering. My confusion lies in why need equivalent Denominator > 200 and is divisible by 2 or 3 can enable dithering? it's very…
Part Number: LMX2581 Table 5 in the data sheet says Approximate (NOT ensured) VCO Core Frequency Ranges. In my design there are boundaries where, as I step in frequency, the VCO core will change. I have identified them according to Table 5. This is not…
Part Number: LMX2581 Other Parts Discussed in Thread: LMX2582 Hello TI Team,
I am planning to use LMX2581 RFPLL in my new design for generating Clocks upto 3.5GHz.
I saw Phase noise plots for some frequencies in Datasheet with Narrow and Wide band…
Part Number: LMX2581 Reading the responses from before, I realize one question was not answered. The earlier post is marked resolved so I am asked this question again. In writing to Reg 6 with LD_SELECT = 4, table 15 shows the register map with RD_DIAGNOSTICS…
Part Number: LMX2581 LD_SELECT can be values from 0 to 15. For number 4, READBACK, you have to clock out the bits for the register you are reading. It appears other bits are just a single logic output such as for LD_SELECT values of 1, 2, or 3 that are…
Part Number: LMX2581 Hi support team
l am reading LMX2581 datasheet and l am confused about primary fractional spur.
primary fractional spur is Fpd/PLL_DEN.For instance, if the phase detector frequency is 100 MHz and the fraction is 3/100, the primary…