Part Number: LMX2581E Other Parts Discussed in Thread: CODELOADER Tool/software: Hello,
we use the LMX2581E in a Downconverter as Local Oscillator (LO). So far I can initialize the unit and set the frequency and the unit is operating well. The frequency…
Part Number: LMX2581E Other Parts Discussed in Thread: LMX2581 Dear Sirs.
I have a question regarding the datasheet of LMX2581, chapter 8.3.13.2. Quotation: "The DLD_ERR_CNT specifies how may errors are necessary to cause the circuit to consider the PLL…
Part Number: LMX2581E Other Parts Discussed in Thread: LMX2572 We are planning to use LMX2581E as local oscillator for our super heterodyne architecture..
We need to generate 140MHZ to 240MHZ output frequency with 25MHZ as reference clock..
The frequency…
Part Number: LMX2581E Hello, I designed a board with an LMX2581E and I can't manage to communicate with it.
I followed the datasheet recommended initialization sequence which suggest when power is good to soft reset the LMX then write from R15 to R0…
Part Number: LMX2581E The LMX2581E uses the RTV mechanical design.
The RTV drawing says "Thermal Pad Size and Shape shown on separate sheet". I cannot find this in either the LMX2581E datasheet or elsewhere.
Is there a recommended footprint…
Part Number: LMX2581E
I'm confused by 8.13.14.2 (serial microwire readback).
It appears as though LD or MUXOUT are constantly being driven with readback data (regardless of LE). Is this the case?
So, if I program MUXOUT_SELECT to be READBACK, the…
Part Number: LMX2581E Other Parts Discussed in Thread: LMX2581 Hello team,
I'd like to know LMX2581 lock frequency accuracy.
In my configuration, VC-TCXO 30.72MHz is used.
The phase noise doesn't look good below 10Hz. So I'm looking for proper setting…
Part Number: LMX2581E In device block diagram, it seems to be that N divider is only for Fin source.
Could N divider, PLL_N, configuration not be used for OSCin source?
Part Number: LMX2581E
Hello!
I use LMX2591E as the LO of the down-conversion receiver, the frequency range is 1690MHz~1990MHz, step 0.25MHz, and the phase noise is abnormal in the range of 1879MHz~1881MHz. 1880MHz is typical as shown in the figure above…