Part Number: LMX2581E Other Parts Discussed in Thread: CDCM6208 Can we generate two different divided frequencies(output of the divider) at the same time in channel A and Channel B?
For example channel A need to be generate 300MHz and channel B need to…
Part Number: LMX2581E Other Parts Discussed in Thread: LMX2581 , , LMX2572 What re the main differences between LMX2581 and LMX2581E?
Is it ONLY the output frequency of 3800M Vs 3760M?
Part Number: LMX2581E Hi,
In my system, the board that hass LMX2581Es mounted is type of Mezzanine board so I plan to have Aluminum thermal boss to be contacted on top of LMX2581E package to flow heat to outer clamshell. Question here is is there any…
Part Number: LMX2581E Other Parts Discussed in Thread: CODELOADER Hi,
I have an Evaluation Module for LMX2581E. Currently I am using TI's CodeLoader software for setting up the device.
But now I need to use Matlab for automatic communication. Is there…
Part Number: LMX2581E Other Parts Discussed in Thread: LMX2581 I would like to use an LMX2581E Synthesizer to create a clock of 93.44 MHz out of a reference clock of 61.38 MHz.
The usual application of LMX2581 is to create an RF signal but I require a…
Part Number: LMX2581E Other Parts Discussed in Thread: LMX2581 , , LMX2572
Hi Team,
Could you please help us explain the difference between LMX2581 and LMX2581E ?
1). What is the background of LMX2581E development ?
2). Are there any performance difference…
Part Number: LMX2581E Hi,
I am trying to design my own board using LMX2581E reference EVM circuit and wondering about CE pin. CE pin doesn't seem to like be used for Microwire programming but still in microwire control line interface. Is CE pin mainly…
Part Number: LMX2581E Hi,
In data sheet, V_IH is rated as 1.4V to Vcc. From my FPGA, LVCMOS18 Voh min. is Vcc-0.45V which is 1.8V-0.45V=1.35V for my application. I want to know if SPI control voltage can support 1.35V as a min. for V_IH. or if this is…
Part Number: LMX2581EVM Other Parts Discussed in Thread: LMX2581E Hi, I am working on schematic capture for LMX2581E but has several questions. My reference schematic is figuure 8 at snau136c.pdf
1) RF output pull up: RF output As used 51ohm resistor between…
Part Number: LMX2581E Hi all,
According to the LMX2581E datasheet, there are two powerdown modes, Partial Powerdown and Full Powerdown. Which powerdown state is IccPD? When coming out of a partial powerdown state, how long will the VCO be operarional? Regards…